I'm having trouble converting my BIOS configuration (.CDB) file to work in CCS4.
CCS4 loaded the legacy CCS3.1 project properly, but did not convert the CDB file.
When I try to directly open the CDB file it pauses for a while and then the configuration tool crashes:
The help file says you can also migrate from BIOS 4.90 to BIOS 5.41 using the CDB2GCF utility. This utility does not exist on my installation of CCS4.
I try to create a new DSP.BIOS 5 configuration file. I choose the dsk6713 since our board uses a 6713 and I see no options to start without a predefined platform. When I hit finish to start the conversion I get::
How do I fix this?
Thanks,
Peter Steinberg