Hello. I have a IP35 camera that has the same DM365-IMX104 software. I want to build the source code to do some modifications. I downloaded the source code from here:

But I have this error:
alg_vnf.c:6:38: error: ti/sdo/codecs/ktnf/iktnf.h: No such file or directory
make[4]: *** [depend] Error 1
I tried to contact with APPRO to obtain a DM365-IMX104 or DM368-IMX104 camera but they don't have in stock.
So, where can I obtain the complete source code? Or in case that it's not possible, where is the iktnf.h file (missed codecs at ti/sdo/codecs)?
Regards