Hi,
I am using DM8148 EVM, with EZSDK _5_05_02_00. I am using CodeSourcery Toolchain arm-2009q1. I want to create a video pipeline in DM8148 using gstreamer through SGX530.
I have gone through the site "http://processors.wiki.ti.com/index.php/GPU_Compositing" . I have the following queries?
1) I want to know if GPU_Compositing is possible in Dm8148?
2) Will EZSDK support it or I have to download AMSDK 5.x?
3) Should I have to use a different cross compiler other than CodeSourcery Toolchain arm-2009q1?
Also if any document is available for GPU_Compositing in Dm8148 .
Regards,
Debasish