Other Parts Discussed in Thread: SYSBIOS
Hi All,
I am starting programing with Tiva-C TM4C1294XL, I just created a project from the TI-RTOS Driver template projects and I enabled the NDK (TCP, IP and HTTP) and FatFS in the configuration.
I did not add new code to the program. When I try to debug the program, I receive the folowing message in the console:
Starting the example
System provider is set to SysMin. Halt the target to view any SysMin contents in ROV.
ti.sysbios.heaps.HeapMem: line 307: out of memory: handle=0x200110fc, size=1804
00000.000 mmBulkAlloc(): could not allocate memory.
00000.000 out of memory: handle=0x0, size=536929020
Service Status: DHCPC : Failed : : 000
ti.sysbios.heaps.HeapMem: line 307: out of memory: handle=0x200110fc, size=2048
xdc.runtime.Error.raise: terminating execution
The Memory Allocation view show me that my program is using 106 Kb Flash and 77 Kb SRAM.
What do I need to do in this case?
Thanks in advance.
Leandro