Other Parts Discussed in Thread: TVP5150, TVP7002
Hi,
I am using DM8168 processor with EZSDK version of 5_05_02_00 and my Linux version is linux-2.6.37-psp04.04.00.01.
I am using the Syslink module syslink_2_20_02_20. While giving software reset in the Linux kernel I am getting the below crash messages:
root@dm816x~:# reboot
Stopping PVR
Stopping telnet daemon.
Stopping Hardware abstraction layer hald
run-parts: /etc/dbus-1/event.d/20hal exited with code 1
Stopping thttpd.
ALSA: Storing mixer settings...
Deconfiguring network interfaces... done.
Stopping syslogd/klogd: stopped syslogd (pid 1320)
stopped klogd (pid 1322)
done
Unloading HDVICP2 Firmware
FIRMWARE: I2cInit will be done by M3
FIRMWARE: Memory map bin file not passed
Usage : firmware_loader <Processor Id> <Location of Firmware> <start|stop> [-mmap <memory_map_file>] [-i2c <0|1>]
===Mandatory arguments===
<Processor Id>
Unable to handle kernel NULL pointer dereference at virtual address 00000010
0: DSP, 1:pgd = c0004000
Video-M3, 2: Vp[00000010] *pgd=00000000ss-M3
<Location of Firmware> fInternal error: Oops: 17 [#1]
last sysfs file: /sys/devices/platform/vpss/video0/nodes
Modules linked in: ti81xxvin ov7725 tvp5150 g_zero ti81xxhdmi ti81xxvo ti81xxfb vpss syslink ipv6 [last unloaded: pvrsrvkm]
CPU: 0 Not tainted (2.6.37 #1)
PC is at notify_shmdrv_isr_callback+0x1c/0xac
LR is at notify_shmdrv_video_isr+0x2c/0x3c
pc : [<c02ed70c>] lr : [<c02ed804>] psr: 60000013
sp : d6633e88 ip : d6633ea8 fp : d6633ea4
r10: 00000004 r9 : c0069510 r8 : 00000004
r7 : 00000000 r6 : 00000000 r5 : 00000000 r4 : 00000000
r3 : 00000004 r2 : 00000009 r1 : 00000004 r0 : 00000000
Flags: nZCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c5387d Table: 95874019 DAC: 00000017
Process kworker/0:1 (pid: 22, stack limit = 0xd66322e8)
Stack: (0xd6633e88 to 0xd6634000)
3e80: 00000004 00000000 fffffffe 00000000 d6633ebc d6633ea8
3ea0: c02ed804 c02ed6fc 00000000 00000000 d6633ee4 d6633ec0 c03b2f8c c02ed7e4
3ec0: c050c40c c050c400 00000004 ffffffff 00000004 00000000 d6633f14 d6633ee8
3ee0: c008ba50 c03b2f64 00000000 c050f7c8 d6633f14 d6741600 00000004 d6633f34
3f00: c050f7c8 d645e600 d6633f2c d6633f18 c008ba88 c008ba08 00000000 c050f880
3f20: d6633f54 d6633f30 c0069558 c008ba74 c03b2fec 00000004 00000000 d6741614
3f40: c050f880 d64ebf80 d6633f8c d6633f58 c0081c38 c006951c d6633f7c 00000000
3f60: c0080cd0 d64ebf80 c050f7c8 00000009 c050f7c8 c050f7c8 d64ebf90 d6632000
3f80: d6633fbc d6633f90 c0082590 c0081a58 00000000 d6633fcc d6447ee0 d64ebf80
3fa0: c00823dc 00000000 00000000 00000000 d6633ff4 d6633fc0 c0086900 c00823e8
3fc0: d6447ee0 00000000 d64ebf80 00000000 d6633fd0 d6633fd0 d6447ee0 c0086874
3fe0: c0072c60 00000013 00000000 d6633ff8 c0072c60 c0086880 bfd57be2 fd7dfb17
Backtrace:
[<c02ed6f0>] (notify_shmdrv_isr_callback+0x0/0xac) from [<c02ed804>] (notify_shmdrv_video_isr+0x2c/0x3c)
r7:00000000 r6:fffffffe r5:00000000 r4:00000004
[<c02ed7d8>] (notify_shmdrv_video_isr+0x0/0x3c) from [<c03b2f8c>] (notifier_call_chain+0x34/0x78)
r5:00000000 r4:00000000
[<c03b2f58>] (notifier_call_chain+0x0/0x78) from [<c008ba50>] (__blocking_notifier_call_chain+0x54/0x6c)
[<c008b9fc>] (__blocking_notifier_call_chain+0x0/0x6c) from [<c008ba88>] (blocking_notifier_call_chain+0x20/0x28)
r8:d645e600 r7:c050f7c8 r6:d6633f34 r5:00000004 r4:d6741600
[<c008ba68>] (blocking_notifier_call_chain+0x0/0x28) from [<c0069558>] (mbox_rx_work+0x48/0xec)
[<c0069510>] (mbox_rx_work+0x0/0xec) from [<c0081c38>] (process_one_work+0x1ec/0x318)
r6:d64ebf80 r5:c050f880 r4:d6741614
[<c0081a4c>] (process_one_work+0x0/0x318) from [<c0082590>] (worker_thread+0x1b4/0x2d0)
[<c00823dc>] (worker_thread+0x0/0x2d0) from [<c0086900>] (kthread+0x8c/0x94)
[<c0086874>] (kthread+0x0/0x94) from [<c0072c60>] (do_exit+0x0/0x5e4)
r7:00000013 r6:c0072c60 r5:c0086874 r4:d6447ee0
Code: e1a06000 f57ff04f e3a04000 e2843004 (e7960103)
irmware binary f---[ end trace 427089550005daf8 ]---
ile
<start|stoUnable to handle kernel paging request at virtual address fffffffc
pgd = c0004000
[fffffffc] *pgd=96bfe021, *pte=00000000, *ppte=00000000
Internal error: Oops: 17 [#2]
last sysfs file: /sys/devices/platform/vpss/video0/nodes
Modules linked in: ti81xxvin ov7725 tvp5150 g_zero ti81xxhdmi ti81xxvo ti81xxfb vpss syslink ipv6 [last unloaded: pvrsrvkm]
CPU: 0 Tainted: G D (2.6.37 #1)
PC is at kthread_data+0x10/0x18
LR is at wq_worker_sleeping+0x14/0x88
pc : [<c0086428>] lr : [<c0083474>] psr: 00000193
sp : d6633c40 ip : d6633c50 fp : d6633c4c
r10: d6499c68 r9 : d6499b78 r8 : d6632000
r7 : d6438000 r6 : d6499ce4 r5 : d6499b80 r4 : 00000000
r3 : 00000000 r2 : 00000040 r1 : 00000000 r0 : d6499b80
Flags: nzcv IRQs off FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c5387d Table: 95874019 DAC: 00000015
Process kworker/0:1 (pid: 22, stack limit = 0xd66322e8)
Stack: (0xd6633c40 to 0xd6634000)
3c40: d6633c64 d6633c50 c0083474 c0086424 ffffffff d6499b80 d6633c8c
Please suggest any solution to solve this issue.
Thanks in advance.
Regards,
Salih