This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X- SDK8.0 failed to load am335x-pm-firmware.elf in the BBB

Other Parts Discussed in Thread: TPS65217

Dear Sir,

I want to test deep sleep mode function, but the BBB power on occur "failed to load am335x-pm-firmware.elf"

I use SDK8.0 "arch/arm/boot/dts/am335x-boneblack.dts" and zImage to bring up the BBB.

INIT: version 2.88 booting
Error opening /dev/fb0: No such file or directory
Starting udev
[    5.289065] udev[833]: starting version 164
[    5.437184]  remoteproc0: failed to load am335x-pm-firmware.elf
[    5.443516]  remoteproc0: powering up wkup_m3
[    5.448131]  remoteproc0: Direct firmware load failed with error -2
[    5.454736]  remoteproc0: Falling back to user helper
[    6.416966] random: nonblocking pool is initialized
[    7.106108]  remoteproc0: request_firmware failed: -2
[    7.111487] wkup_m3 44d00000.wkup_m3: rproc_boot failed
[    7.915121] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.

Please help provide the suggestion for the question, thanks.


B.R.

Joe

PS: Detailed log as below

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 3.14.26-g07d13c6-dirty (joe@jhr330) (gcc version 4.7.3 201302                                                                   26 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #                                                                   52 Thu Mar 12 11:57:21 CST 2015
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: TI AM335x BeagleBone
[    0.000000] cma: CMA: reserved 24 MiB at 9e000000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM335X ES2.1 (sgx neon )
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129536
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfsty                                                                   pe=ext4 rootwait
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 484260K/522240K available (5787K kernel code, 313K rwdata, 2088K ro                                                                   data, 269K init, 231K bss, 37980K reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc07b9054   (7877 kB)
[    0.000000]       .init : 0xc07ba000 - 0xc07fd414   ( 270 kB)
[    0.000000]       .data : 0xc07fe000 - 0xc084c720   ( 314 kB)
[    0.000000]        .bss : 0xc084c720 - 0xc08866f8   ( 232 kB)
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[    0.000000] Total of 128 interrupts on 1 active controller
[    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[    0.000012] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
[    0.000029] OMAP clocksource: timer1 at 24000000 Hz
[    0.000249] Console: colour dummy device 80x30
[    0.000275] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[    0.089562] pid_max: default: 32768 minimum: 301
[    0.089647] Security Framework initialized
[    0.089695] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.089703] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[    0.095245] CPU: Testing write buffer coherency: ok
[    0.095585] Setting up static identity map for 0x805acfe0 - 0x805ad038
[    0.096379] devtmpfs: initialized
[    0.097875] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[    0.103535] omap_hwmod: tptc0 using broken dt data from edma
[    0.103602] omap_hwmod: tptc1 using broken dt data from edma
[    0.103659] omap_hwmod: tptc2 using broken dt data from edma
[    0.107585] omap_hwmod: debugss: _wait_target_disable failed
[    0.162088] pinctrl core: initialized pinctrl subsystem
[    0.162954] regulator-dummy: no parameters
[    0.164956] NET: Registered protocol family 16
[    0.166582] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.168677] cpuidle: using governor ladder
[    0.168691] cpuidle: using governor menu
[    0.174112] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] register                                                                   ed
[    0.175339] platform 49000000.edma: alias fck already exists
[    0.175362] platform 49000000.edma: alias fck already exists
[    0.175374] platform 49000000.edma: alias fck already exists
[    0.176345] OMAP GPIO hardware version 0.1
[    0.187776] No ATAGs?
[    0.187797] hw-breakpoint: debug architecture 0x4 unsupported.
[    0.208466] bio: create slab <bio-0> at 0
[    0.221068] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[    0.221900] vmmcsd_fixed: 3300 mV
[    0.224287] vgaarb: loaded
[    0.224729] i2c-core: driver [palmas] using legacy suspend method
[    0.224738] i2c-core: driver [palmas] using legacy resume method
[    0.225337] SCSI subsystem initialized
[    0.226549] usbcore: registered new interface driver usbfs
[    0.226704] usbcore: registered new interface driver hub
[    0.226872] usbcore: registered new device driver usb
[    0.227644] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pin                                                                   mux_i2c0_pins, deferring probe
[    0.227668] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
[    0.227690] omap_i2c 4802a000.i2c: could not find pctldev for node /pinmux@44e10800/pin                                                                   mux_i2c1_pins, deferring probe
[    0.227702] platform 4802a000.i2c: Driver omap_i2c requests probe deferral
[    0.228002] pps_core: LinuxPPS API ver. 1 registered
[    0.228011] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giome                                                                   tti@linux.it>
[    0.228124] PTP clock support registered
[    0.229783] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[    0.230504] Advanced Linux Sound Architecture Driver Initialized.
[    0.231849] Switched to clocksource timer1
[    0.247645] NET: Registered protocol family 2
[    0.248343] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[    0.248387] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[    0.248424] TCP: Hash tables configured (established 4096 bind 4096)
[    0.248481] TCP: reno registered
[    0.248492] UDP hash table entries: 256 (order: 0, 4096 bytes)
[    0.248507] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[    0.248666] NET: Registered protocol family 1
[    0.249025] RPC: Registered named UNIX socket transport module.
[    0.249037] RPC: Registered udp transport module.
[    0.249042] RPC: Registered tcp transport module.
[    0.249048] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.249936] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters availabl                                                                   e
[    0.252254] futex hash table entries: 256 (order: -1, 3072 bytes)
[    0.388709] VFS: Disk quotas dquot_6.5.2
[    0.388766] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.389203] NFS: Registering the id_resolver key type
[    0.389271] Key type id_resolver registered
[    0.389278] Key type id_legacy registered
[    0.389312] jffs2: version 2.2. (NAND) (SUMMARY)  ? 2001-2006 Red Hat, Inc.
[    0.389462] msgmni has been set to 993
[    0.390639] NET: Registered protocol family 38
[    0.390673] io scheduler noop registered
[    0.390680] io scheduler deadline registered
[    0.390703] io scheduler cfq registered (default)
[    0.392190] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[    0.397273] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[    0.399789] omap_uart 44e09000.serial: no wakeirq for uart0
[    0.399921] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) i                                                                   s a OMAP UART0
[    1.056327] console [ttyO0] enabled
[    1.060548] omap_uart 48022000.serial: no wakeirq for uart0
[    1.071722] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 89, base_baud = 3000000) i                                                                   s a OMAP UART1
[    1.082607] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[    1.089849] [drm] Initialized drm 1.1.0 20060810
[    1.103561] brd: module loaded
[    1.111213] loop: module loaded
[    1.114895] (hci_tty): inside hci_tty_init
[    1.119559] (hci_tty): allocated 249, 0
[    1.125754] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.135543] usbcore: registered new interface driver asix
[    1.141373] usbcore: registered new interface driver ax88179_178a
[    1.147910] usbcore: registered new interface driver cdc_ether
[    1.154203] usbcore: registered new interface driver smsc95xx
[    1.160371] usbcore: registered new interface driver net1080
[    1.166428] usbcore: registered new interface driver cdc_subset
[    1.172775] usbcore: registered new interface driver zaurus
[    1.178826] usbcore: registered new interface driver cdc_ncm
[    1.185162] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.192020] ehci-pci: EHCI PCI platform driver
[    1.196832] ehci-omap: OMAP-EHCI Host Controller driver
[    1.202704] usbcore: registered new interface driver cdc_wdm
[    1.208802] usbcore: registered new interface driver usb-storage
[    1.215991] mousedev: PS/2 mouse device common for all mice
[    1.223388] i2c-core: driver [rtc-ds1307] using legacy suspend method
[    1.230135] i2c-core: driver [rtc-ds1307] using legacy resume method
[    1.237550] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[    1.245695] i2c /dev entries driver
[    1.249479] Driver for 1-wire Dallas network protocol.
[    1.256843] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    1.374548] ledtrig-cpu: registered to indicate activity on CPUs
[    1.381159] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[    1.388352] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[    1.395765] usbcore: registered new interface driver usbhid
[    1.401629] usbhid: USB HID core driver
[    1.405939] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[    1.413468] mmc0: host does not support reading read-only switch. assuming write-enable                                                                   .
[    1.423066] mmc0: new SD card at address 92aa
[    1.428911] mmcblk0: mmc0:92aa SU01G 968 MiB
[    1.435299] oprofile: using arm/armv7
[    1.439286]  mmcblk0: p1 p2
[    1.443024] TCP: cubic registered
[    1.446500] Initializing XFRM netlink socket
[    1.450981] NET: Registered protocol family 17
[    1.456389] NET: Registered protocol family 15
[    1.461199] Key type dns_resolver registered
[    1.469446] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/volt                                                                   dm: -517
[    1.478593] cpu cpu0: cpu0 clock notifier not ready, retry
[    1.484435] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[    1.492854] PM: bootloader does not support rtc-only!
[    1.498246] ThumbEE CPU extension supported.
[    1.502821] Registering SWP/SWPB emulation handler
[    1.509335] regulator-dummy: disabling
[    1.518613] tilcdc 4830e000.lcdc: no encoders/connectors found
[    1.524849] tilcdc 4830e000.lcdc: failed to initialize mode setting
[    1.541309] DCDC1: at 1500 mV
[    1.545542] vdd_mpu: 925 <--> 1375 mV at 1325 mV
[    1.551431] vdd_core: 925 <--> 1150 mV at 1125 mV
[    1.557555] LDO1: at 1800 mV
[    1.561714] LDO2: at 3300 mV
[    1.565828] LDO3: 1800 mV
[    1.569617] LDO4: at 3300 mV
[    1.573131] mmc1: BKOPS_EN bit is not set
[    1.578034] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[    1.583672] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[    1.591090] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[    1.597683]  remoteproc0: wkup_m3 is available
[    1.602396]  remoteproc0: Note: remoteproc is still under development and considered ex                                                                   perimental.
[    1.611777]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatib                                                                   ility isn't yet guaranteed.
[    1.622789]  remoteproc0: Direct firmware load failed with error -2
[    1.629361]  remoteproc0: Falling back to user helper
[    1.635113] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[                                                                   950000<->1325000]:-22
[    1.646378] mmc1: new high speed MMC card at address 0001
[    1.667175] mmcblk1: mmc1:0001 MMC04G 3.60 GiB
[    1.672076] mmcblk1boot0: mmc1:0001 MMC04G partition 1 2.00 MiB
[    1.678724] mmcblk1boot1: mmc1:0001 MMC04G partition 2 2.00 MiB
[    1.686051]  mmcblk1: p1 p2
[    1.690971]  mmcblk1boot1: unknown partition table
[    1.697468]  mmcblk1boot0: unknown partition table
[    1.721894] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[    1.728280] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[    1.735460] libphy: 4a101000.mdio: probed
[    1.739667] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LA                                                                   N8710/LAN8720
[    1.750034] cpsw 4a100000.ethernet: Detected MACID = 6c:ec:eb:68:fa:f4
[    1.758501] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:00 UTC (946                                                                   684800)
[    1.770108] ALSA device list:
[    1.773285]   No soundcards found.
[    1.780117] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[    1.787832] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[    4.347191] EXT4-fs (mmcblk0p2): recovery complete
[    4.502667] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null                                                                   )
[    4.511259] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[    4.524660] devtmpfs: mounted
[    4.529154] Freeing unused kernel memory: 268K (c07ba000 - c07fd000)
INIT: version 2.88 booting
Error opening /dev/fb0: No such file or directory
Starting udev
[    5.289065] udev[833]: starting version 164
[    5.437184]  remoteproc0: failed to load am335x-pm-firmware.elf
[    5.443516]  remoteproc0: powering up wkup_m3
[    5.448131]  remoteproc0: Direct firmware load failed with error -2
[    5.454736]  remoteproc0: Falling back to user helper
[    6.416966] random: nonblocking pool is initialized
[    7.106108]  remoteproc0: request_firmware failed: -2
[    7.111487] wkup_m3 44d00000.wkup_m3: rproc_boot failed
[    7.915121] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be cor                                                                   rupt. Please run fsck.
ERROR: could not open directory /lib/modules/3.14.26-g07d13c6-dirty: No such file or direc                                                                   tory
WARNING: -e needs -E or -F
ERROR: could not open directory /lib/modules/3.14.26-g07d13c6-dirty: No such file or direc                                                                   tory
FATAL: could not search modules: No such file or directory
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file or directory
bootlogd.
[    8.133918] EXT4-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck i                                                                   s recommended
[    8.149012] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered
ALSA: Restoring mixer settings...
Configuring network interfaces... /usr/sbin/alsactl: load_state:1686: No soundcards found.                                                                   ..
[    8.711507] net eth0: initializing cpsw version 1.12 (0)
[    8.792607] net eth0: phy found : id is : 0x7c0f1
[    8.797593] libphy: PHY 4a101000.mdio:01 not found
[    8.802627] net eth0: phy 4a101000.mdio:01 not found on slave 1
udhcpc (v1.20.2) started
Sending discover...
[   11.895238] libphy: 4a101000.mdio:00 - Link is Up - 100/Full
Sending discover...
Sending select for 192.168.1.12...
Lease of 192.168.1.12 obtained, lease time 86400
/etc/udhcpc.d/50default: Adding DNS 192.168.1.10
done.
Wed Jun 26 03:48:00 UTC 2013
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Performing wifi calibration...
rm: can't remove '/lib/firmware/ti-connectivity/wl1271-nvs.bin': No such file or directory
Error: Module wl12xx_sdio is not currently loaded
nl80211 not found.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
Starting Lighttpd Web Server: 2013-06-26 03:48:00: (log.c.166) server started
lighttpd.
/
Starting Matrix GUI application.
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
        binutils-symlinks
        binutils
        gdbserver

If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.

 _____                    _____           _         _
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
              |___|                    |___|

Arago Project http://arago-project.org am335x-evm ttyO0

Arago 2013.05 am335x-evm ttyO0

am335x-evm login: