This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Just trying to address any errors I see in the boot log of the kernel and I'm down to the last two errors;
root: mount: mounting rootfs on / failed: No such file or directory
root: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
Are these because the /etc/fstab file is trying to mount these files? If so I understand why the usbfs won't work as i have not included that in my driver and no usb device is present... however i dont understand the first error. Of course my file system is mounted at /, and i can see that using the ls command. Is this line necessary? What is it trying to do? Can i remove this line in fstab in the filesystem?
Here is the fstab file:
root@arago:/etc# cat fstab
# stock fstab - you probably want to override this with a machine specific one
rootfs / auto defaults 1 1
proc /proc proc defaults 0 0
devpts /dev/pts devpts mode=0620,gid=5 0 0
usbfs /proc/bus/usb usbfs defaults 0 0
tmpfs /var/volatile tmpfs defaults,size=16M 0 0
tmpfs /dev/shm tmpfs mode=0777 0 0
tmpfs /media/ram tmpfs defaults,size=16M 0 0
# uncomment this if your device has a SD/MMC/Transflash slot
#/dev/mmcblk0p1 /media/card auto defaults,sync,noauto 0 0
root@arago:/etc#
And this is the whole boot log;
Booting with TI UBL
Device OPP (300MHz, 1.2V)
Booting Catalog Boot Loader
BootMode = SPI 1 Flash
32 bit Address
Copying U-Boot from SPI to 0xC1008000...
FHB Validated ... Complete
Copying FileSystem from SPI to 0xC1800000...
FHB Validated ... Complete
Copying uImage from SPI to 0xC3000000...
FHB Validated ... Complete
All images validated and loaded.
Jumping to entry point at at 0xC1080000...
U-Boot 2012.04.01-svn2238 (Mar 06 2015 - 10:22:10)
DRAM: 64 MiB
WARNING: Caches not enabled
Using default environment
In: serial
Out: serial
Err: serial
Net: DaVinci-EMAC
Hit any key to stop autoboot: 0
## Booting kernel from Legacy Image at c3000000 ...
Image Name: Linux-3.19.0-rc5-svn2308
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2026352 Bytes = 1.9 MiB
Load Address: c1008000
Entry Point: c1008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
Booting Linux on physical CPU 0x0
Linux version 3.19.0-rc5-svn2308 (dan@DWAYER-UBUNTU) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #8 PREEMPT Thu Mar 12 13:42:24 CDT 2015
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=0005317f
CPU: VIVT data cache, VIVT instruction cache
Machine: AMSC NGCC board
Ignoring memory below PHYS_OFFSET: 0xc0000000-0xc1000000
Memory policy: Data cache writethrough
DaVinci da850/amsc-ngcc/am18x variant 0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 12192
Kernel command line: mem=48M@0xC1000000 console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0xC1800000,4MB
PID hash table entries: 256 (order: -2, 1024 bytes)
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 39220K/49152K available (2882K kernel code, 199K rwdata, 944K rodata, 156K init, 1138K bss, 9932K reserved, 0K cma-reserved)
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xc3800000 - 0xff000000 ( 952 MB)
lowmem : 0xc0000000 - 0xc3000000 ( 48 MB)
modules : 0xbf000000 - 0xc0000000 ( 16 MB)
.text : 0xc0008000 - 0xc03c4ecc (3828 kB)
.init : 0xc03c5000 - 0xc03ec000 ( 156 kB)
.data : 0xc03ec000 - 0xc041dc60 ( 200 kB)
.bss : 0xc041dc60 - 0xc053a4ec (1139 kB)
SLUB: HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
NR_IRQS:245
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
Console: colour dummy device 80x30
Calibrating delay loop... 226.09 BogoMIPS (lpj=1130496)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
Setting up static identity map for 0xc12d6c10 - 0xc12d6c68
devtmpfs: initialized
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
edma-dma-engine edma-dma-engine.1: TI EDMA DMA engine driver
Switched to clocksource timer0_1
NET: Registered protocol family 2
TCP established hash table entries: 1024 (order: 0, 4096 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 1024 bind 1024)
TCP: reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 4096K (c0800000 - c0c00000)
futex hash table entries: 256 (order: -1, 3072 bytes)
io scheduler noop registered (default)
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
console [ttyS0] disabled
serial8250.0: ttyS0 at MMIO 0x1c42000 (irq = 25, base_baud = 14250000) is a 16550A
console [ttyS0] enabled
brd: module loaded
spi_davinci spi_davinci.1: DMA: supported
spi_davinci spi_davinci.1: DMA: RX channel: 0x00000012, TX channel: 0x00000013, event queue: 0
m25p80 spi1.0: found n25q256a, expected n25q512a
m25p80 spi1.0: n25q256a (32768 Kbytes)
Creating 15 MTD partitions on "m25p80":
0x000000000000-0x000000040000 : "Stage1"
0x000000040000-0x000000140000 : "Stage2"
0x000000140000-0x000000180000 : "NVRAM"
0x000000180000-0x0000001c0000 : "Mfg Dflts"
0x0000001c0000-0x000000200000 : "Params"
0x000000200000-0x000000300000 : "Stage3"
0x000000300000-0x000000500000 : "FPGA"
0x000000500000-0x000000900000 : "TestAppDSP"
0x000000900000-0x000000d00000 : "AppDSP"
0x000000d00000-0x000000d40000 : "TestAppParams"
0x000000d40000-0x000000d80000 : "UBL"
0x000000d80000-0x000000e80000 : "U-boot"
0x000000e80000-0x000001280000 : "UImage"
0x000001280000-0x000001880000 : "LinuxInitFS"
0x000001880000-0x000001c80000 : "LinuxUserFS"
spi_davinci spi_davinci.1: Controller at 0xfef0e000
omap_rtc da830-rtc: already running
omap_rtc da830-rtc: rtc core: registered da830-rtc as rtc0
i2c /dev entries driver
TCP: cubic registered
NET: Registered protocol family 17
console [netcon0] enabled
netconsole: network logging started
omap_rtc da830-rtc: setting system clock to 2000-01-01 00:20:56 UTC (946686056)
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing unused kernel memory: 156K (c03c5000 - c03ec000)
INIT: version 2.86 booting
Please wait: booting...
Starting udev
WARNING: -e needs -E or -F
random: nonblocking pool is initialized
Remounting root file system...
Caching udev devnodes
Populating dev cache
root: mount: mounting rootfs on / failed: No such file or directory
root: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
done.
Setting up IP spoofing protection: rp_filter.
Tue Aug 5 19:16:00 UTC 2014
INIT: Entering runlevel: 5
Starting telnet daemon.
Starting syslogd/klogd: done
Copying userfs from /dev/mtd14 to /usr/userfs.tar.gz... Attempting to open /dev/mtd14 device!
File access to /dev/mtd14 created!
Attempting to open /usr/userfs.tar.gz !
/usr/userfs.tar.gz created!
Attempting to read /dev/mtd14 !
Read from /dev/mtd14 succeeded !
magic: 0x42484641
infoBlockOffset: 0x0000468A
infoBlockLength: 0x00000410
infoBlockSignature: 0x4017096D
imageOffset: 0x00000020
imageLength: 0x0000466A
imageSignature: 0x5BEE4049
fhbSignature: 0xC351301C
FHB Magic Number correct
FHB CRC correct
FHB read successfully
Program image copied successfully!
Image CRC correct
Program image read successfully
Closing file: /usr/userfs.tar.gz !
Closing file: /dev/mtd14 !
Complete.
User Application Starting...
Hello World, from the user application!
User Application Complete...
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org arago ttyS0
Arago 2011.09 arago ttyS0
arago login: