Hi,
On our custom DM6446 processor board, The TFTP kernel load showing odd behaviour. The command is randomly getting success after multiple re-boots.
the log is as shown below.
U-Boot >tftp 0x80700000 uImage_r37_NAND2
TFTP from server 201.123.80.154; our IP address is 201.123.80.239
Filename 'uImage_r37_NAND2'.
Load address: 0x80700000
Loading: *#################################################################
###################T T T T T T T
re-booted.
U-Boot >tftp 0x80700000 uImage_r37_NAND2
TFTP from server 201.123.80.154; our IP address is 201.123.80.239
Filename 'uImage_r37_NAND2'.
Load address: 0x80700000
Loading: *T T T T T T T T T T T T T T
rebooted.
U-Boot > tftp 0x80700000 uImage_r37_NAND2
TFTP from server 201.123.80.154; our IP address is 201.123.80.239
Filename 'uImage_r37_NAND2'.
Load address: 0x80700000
Loading: *#################################################################
############T #####################################################
###
done
Bytes transferred = 1942584 (1da438 hex)
re-booted.
U-Boot > tftp 0x80700000 uImage_r37_NAND2
TFTP from server 201.123.80.154; our IP address is 201.123.80.239
Filename 'uImage_r37_NAND2'.
Load address: 0x80700000
Loading: *#################################################################
#################################################################
###
done
Bytes transferred = 1942584 (1da438 hex)
The NFS connection is also some time successfull and some time failure.
where may be the problem?
Thanks,
Satish.