hi - i'm trying to install the PRU addin package on top of the SDK am335x evm (7.00.00.00 ) on an Ubuntu 12.10 machine. i have two current problems: the first is i'm trying to reinstall the SDK 7.00 but it appears only the 8.00.00.00 version is available. I want to install a fresh copy because i can't get the PRU add in to recognize the SDK folder. is there a link where SDK am335x evm 7.00.00.00 linux is available? the second problem is that, using the copy i do have, i try to install the PRU addon v1 linux and it asks for the install target for SDK i'm using. I navigate to that folder and select it (or type it in, depending on which of the many times i've tried this). i then click "forward" and it tells me it's a invalid SDK directory. i have never gotten past this point. since the prior screen only offers me a selection for the v7 of the SDK, and not the v8 version, i hope there is an update coming soon. I've installed using sudo so i don't think it's a permission problem. any suggestions?
thanks,
Jim