This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booting the DM355



I am working on my own DM355 board, and I have not been able to get it to show me the BOOTME message when I try to get it to boot from UART. I wanted to ask you if you could suggest possible causes for this (other than those I have not considered.)

The possible causes I am currently checking are the following:
1) Power supply currents, timing, ripple.
2) Board power supply and GND connections.
3) XTAL issues
4) UART connections and RS-232 to 3.3VTLL conversion.
5) Appropriate configuration pins (BTSEL[1:0])

My assumption here (I would particularly appreciate if you can confirm this is correct) is that IF there could be an error on USB, SD, External RAM, External Flash or Video decoder, it would NOT affect the first step in getting the DM355 to show BOOTME through UART.

An additional piece of information is that I was actually able to Program the Flash memory through JTAG (at least that is what CCS claims), but the system did not boot anyway.