This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Low priority task making high priority task to halt



Hi,

I'm using SYS/BIOS v6.33.6.50 on TI DSP C6674.

I had an application with 3 tasks, task 1 - Ethernet Ping (Priority : 15), task 2 - Simple UART application (Priority : 5), task 3 - an application processing (Priority : 4).

My task 3 is added recently, before that only two task (1,2) present and Ethernet PING is successfully received.

After adding task 3 which is responsible to process the data continuously so added it in while loop, With this while loop it is observed that Ethernet ping response is not coming.

If i disable task 3, then everything goes right with Ethernet PING.

I want your inputs on how to run a low priority task with continuous loop, without effecting high priority task behavior.

Awaiting for your inputs.

Thanks

Mani Kumar