Other Parts Discussed in Thread: TMS320C6657
Hello, any app note or information as how to interface the TMS320C6657 such as the Lite Evaluation Module to a camera?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320C6657
Hello, any app note or information as how to interface the TMS320C6657 such as the Lite Evaluation Module to a camera?
Hi Mahdavi,
Welcome to the TI E2E forum. I hope you will find many good answers here and in the TI.com documents and in the TI Wiki Pages (for processor issues). Be sure to search those for helpful information and to browse for the questions others may have asked on similar topics (e2e.ti.com).
From my understanding, We don't have app note and keystone EVM's does not support to interface camera. Please refer below thread for more information,
e2e.ti.com/.../379769
Thank you.
So the question is how to tranfer the data from them to TMS320C6657 EVM. Any idea?
The camera can be connected to Windows/Linux based host through USB/Ethernet and C6657 EVM can be connected through PCIe slot using adaptor card. With this configuration, image data can be read using camera SDK and can be send to DSP for processing via PCIe using MCSDK 2.x.
Do you think installing SYS/BIOS and Linux MCSDK on EVM would allow us to connect to these cameras through USB or Ethernet?
The Multicore Software Development Kit (MCSDK) provides the core foundational building blocks that facilitate application software development on TI's high performance and multicore DSPs. The MCSDK & CCS will be installed on Windows/Linux based host not on EVM for application development for C66xx devices.
Thanks Raja. We'd like to have a stand alone solution without PC so going through PCI is not an option. We want to capture the image sensor data in raw mode and from my research it seems Video Port is what we need and DaVinci DSPs have it. However, in this application we possibly dont need any ARM processor. So, to keep it simple just a C6-like DSP is preffered. App note SPRU629G talks about Video Ports of C64x but does not say which ones have it. Is there a C64 DSP or DaVinci without ARM available with video port?
Hello Pourang,
The video port is available in Davinci devices like DM647 (DSP only) device and available for C64x devices. Please refer table 2 in below reference guide.

Regards,
Senthil