This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FFTC ifft operation issue

Hello,

currently i am implementing ifft operation using FFTC(FFTC Driver version: 0x1000010 Version Info: FFTC Driver Revision: 01.00.00.16) on the C6670 EVM and ran into an issue. 

I modified the test_singlecore_poll.c slightly to reproduce this issue. Initially the test reads inputdata(A) and expected outputdata(B), then it does a 2048 FFT operation on inputdata A and checks the result with the expected data B. This test passes fine.

What i did now is to configure FFTC to do IFFT operation and changed it to copy outputdata B as input into the descriptorbuffer, so i expected as result to receive A with some different scaling. As a next step i saved buffers A, B and ifft result buffer(C) after receiving the ifft result and imported them into matlab. There i can easily verify, that

fft(A) = B

ifft(B) = A

C != A

but i figured out following equation swap(ifft(swap(B))) = C, where swap() denotes an IQ-swap.

So if we are doing IFFT operation on the DSP the IQ-layout seems to change.

Can someone confirm this issue or am i missing some more configurations to enable ifft operation?

Kind regards

Ralf