HI,
I migrated the latest VLIB(version _3_2_0_2) to ezsdk_evm814x_5_2.
I added the vlib.h into the examples of viddec_copy,but compiled error, with "error invalid target".
I checked the header files ,I found that each file didn't define the C674.
So,how can i compile VLIB on DM8148 with C674x.Any suggestion would be helpful,Thanks.
#ifndef _VLIB_AFAST_NONMAXSUPPRESSION_H_
#define _VLIB_AFAST_NONMAXSUPPRESSION_H_ 1
#if defined (_TMS320C6600)
#include "c66/VLIB_aFast_nonmaxSuppression.h"
#elif defined (_TMS320C6400_PLUS)
#include "c64P/VLIB_aFast_nonmaxSuppression.h"
#else
#error invalid target
#endif
#endif /* _VLIB_AFAST_NONMAXSUPPRESSION_H_ */