This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building AMSDK 8.0 from source

Hello,


We are trying to build AMSDK 8.0 rootfs from source. We are using  the following steps:

$ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh  -f configs/amsdk/amsdk-08.00.00.00-config.txt
$ cd build
$ . conf/setenv
$ export PATH=$HOME/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin:$PATH
$ MACHINE=beaglebone bitbake tisdk-rootfs-image

This unfortunately fails due to the following error:

fatal: Could not read from remote repository.

Please make sure you have the correct access rights
and the repository exists.

ERROR: Function failed: Fetcher failure for URL: 'git://gitorious.org/uim/uim.git'. Unable to fetch URL from any source.

Also, the config.txt does not include git repository HASH that was used to build AMSDK 8.0 release binaries. Is there a way to obtain this information? This hash is especially useful since meta-qt5 in config.txt is set to track 'master' branch, which has changed since the official 8.0 release.

Thanks,

Mikhail