This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Arago compilation broken when moving to "daisy"

Hello,

II tried to update a working Arago installation moving to "daisy" to have more recent files, with the results that nothing works anyomore!

I used the standard command to prepare the "build" directory as in "http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment",

  • Look like my message was cut:

    Whe I launch MACHINE=am437x-evm bitbake core-image-minimal I get this error:

    | configure: exit 0
    | ERROR: oe_runconf failed
    | WARNING: exit code 1 from a shell command.
    | ERROR: Function failed: do_configure (log file is located at /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/temp/log.do_configure.1846)
    ERROR: Task 298 (virtual:native:/calcul/arago/sources/oe-core/meta/recipes-devtools/autoconf/autoconf_2.69.bb, do_configure) failed with exit code '1'


    Does it mean I need to ask thr sysadmin to update autoconf? I'll try adding the log file....
  • DEBUG: Executing python function sysroot_cleansstate
    DEBUG: Python function sysroot_cleansstate finished
    DEBUG: Executing shell function autotools_preconfigure
    Previously configured separate build directory detected, cleaning /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/build
    DEBUG: Shell function autotools_preconfigure finished
    DEBUG: Executing python function autotools_copy_aclocals
    DEBUG: Python function autotools_copy_aclocals finished
    DEBUG: Executing shell function do_configure
    NOTE: Running /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/configure  --build=x86_64-linux           --host=x86_64-linux           --target=x86_64-linux           --prefix=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr           --exec_prefix=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr           --bindir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin           --sbindir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin           --libexecdir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib/autoconf           --datadir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share           --sysconfdir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/etc           --sharedstatedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/com           --localstatedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/var           --libdir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib           --includedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include           --oldincludedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include           --infodir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/info           --mandir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/man           --disable-silent-rules           --disable-dependency-tracking             ac_cv_path_M4=m4
    configure: WARNING: unrecognized options: --disable-silent-rules, --disable-dependency-tracking
    configure: loading site script /calcul/arago/sources/oe-core/meta/site/native
    checking for a BSD-compatible install... /usr/bin/install -c
    checking whether build environment is sane... yes
    checking for a thread-safe mkdir -p... /bin/mkdir -p
    checking for gawk... gawk
    checking whether make sets $(MAKE)... yes
    configure: error: source directory already configured; run "make distclean" there first
    Configure failed. The contents of all config.log files follows to aid debugging
    /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/config.log
    This file contains any messages produced by compilers while
    running configure, to aid debugging if configure makes a mistake.

    It was created by GNU Autoconf configure 2.69, which was
    generated by GNU Autoconf 2.69.  Invocation command line was

      $ /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/configure --build=x86_64-linux --host=x86_64-linux --target=x86_64-linux --prefix=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr --exec_prefix=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr --bindir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin --sbindir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin --libexecdir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib/autoconf --datadir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share --sysconfdir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/etc --sharedstatedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/com --localstatedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/var --libdir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib --includedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include --oldincludedir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include --infodir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/info --mandir=/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/man --disable-silent-rules --disable-dependency-tracking ac_cv_path_M4=m4

    ## --------- ##
    ## Platform. ##
    ## --------- ##

    hostname = cimepe36
    uname -m = x86_64
    uname -r = 3.2.0-4-amd64
    uname -s = Linux
    uname -v = #1 SMP Debian 3.2.57-3+deb7u2

    /usr/bin/uname -p = unknown
    /bin/uname -X     = unknown

    /bin/arch              = unknown
    /usr/bin/arch -k       = unknown
    /usr/convex/getsysinfo = unknown
    /usr/bin/hostinfo      = unknown
    /bin/machine           = unknown
    /usr/bin/oslevel       = unknown
    /bin/universe          = unknown

    PATH: /calcul/arago/sources/oe-core/scripts/native-intercept
    PATH: /calcul/arago/sources/oe-core/scripts
    PATH: /calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/cortexa9hf-vfp-neon-3.8-linux
    PATH: /calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin
    PATH: /calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin
    PATH: /calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin
    PATH: /calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin
    PATH: /calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux//bin
    PATH: /calcul/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin
    PATH: /calcul/arago/sources/bitbake/bin
    PATH: /tima/portolan/bin
    PATH: /softslin/vivado2013_2_0616_1/Vivado/2013.2//bin/
    PATH: /softslin/ise_edk_146i/14.6/ISE_DS/EDK//gnu/arm/lin/bin/
    PATH: /softslin/ise_edk_146i/14.6/ISE_DS/PlanAhead/bin/
    PATH: /softslin/ise_edk_146i/14.6/ISE_DS/EDK//bin/lin
    PATH: /softslin/ise_edk_146i/14.6/ISE_DS/EDK//gnu/powerpc-eabi/lin/bin/
    PATH: /softslin/ise_edk_146i/14.6/ISE_DS/ISE//bin/lin
    PATH: /usr/local/bin
    PATH: /usr/bin
    PATH: /bin
    PATH: /usr/local/games
    PATH: /usr/games
    PATH: /tima/portolan/bin
    PATH: /softslin/modelsim10_0b/modeltech/linux_rh60
    PATH: /tima-fmr/michele/u-boot-xlnx/tools/
    PATH: /softslin/altera11_1/quartus/bin/
    PATH: /tima/portolan/bin/binutils
    PATH: /calcul/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin


    ## ----------- ##
    ## Core tests. ##
    ## ----------- ##

    configure:1796: checking for a BSD-compatible install
    configure:1864: result: /usr/bin/install -c
    configure:1875: checking whether build environment is sane
    configure:1925: result: yes
    configure:2066: checking for a thread-safe mkdir -p
    configure:2105: result: /bin/mkdir -p
    configure:2118: checking for gawk
    configure:2134: found /usr/bin/gawk
    configure:2145: result: gawk
    configure:2156: checking whether make sets $(MAKE)
    configure:2178: result: yes
    configure:2263: checking build system type
    configure:2277: result: x86_64-pc-linux-gnu
    configure:2297: checking host system type
    configure:2310: result: x86_64-pc-linux-gnu
    configure:2337: autobuild project... GNU Autoconf
    configure:2343: autobuild revision... 2.69
    configure:2348: autobuild hostname... cimepe36
    configure:2359: autobuild timestamp... 20140717T103707Z
    configure:2387: checking whether /bin/sh -n is known to work
    configure:2406: result: no
    configure:2410: checking for characters that cannot appear in file names
    configure:2430: result: none
    configure:2436: checking whether directories can have trailing spaces
    configure:2450: result: yes
    configure:2461: checking for expr
    configure:2479: found /usr/bin/expr
    configure:2491: result: /usr/bin/expr
    configure:2510: checking for GNU M4 that supports accurate traces
    configure:2559: result: m4
    configure:2562: checking whether m4 accepts --gnu
    configure:2572: result: yes
    configure:2589: checking how m4 supports trace files
    configure:2599: result: --debugfile
    configure:2623: checking for perl
    configure:2641: found /usr/bin/perl
    configure:2654: result: /usr/bin/perl
    configure:2673: checking whether /usr/bin/perl Fcntl::flock is implemented
    configure:2687: result: yes
    configure:2705: checking for emacs
    configure:2721: found /usr/bin/emacs
    configure:2732: result: emacs
    configure:2750: checking whether emacs is sufficiently recent
    configure:2760: $TEST_EMACS -batch -q -f batch-byte-compile conftest.el 1>&2
    Loading 00debian-vars...
    Loading /etc/emacs/site-start.d/50a2ps.el (source)...
    Loading /etc/emacs/site-start.d/50autoconf.el (source)...
    Loading /etc/emacs/site-start.d/50cmake-data.el (source)...
    Loading /etc/emacs/site-start.d/50dictionaries-common.el (source)...
    Loading debian-ispell...
    Loading /var/cache/dictionaries-common/emacsen-ispell-default.el (source)...
    Loading /var/cache/dictionaries-common/emacsen-ispell-dicts.el (source)...
    Loading /etc/emacs/site-start.d/50psvn.el (source)...

    In broken-mode:
    conftest.el:2:35:Warning: assignment to free variable `broken-defaults'
    Wrote /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/conftest.elc
    configure:2763: $? = 0
    configure:2771: result: yes
    configure:2788: checking for emacs
    configure:2815: result: emacs
    configure:2839: checking where .elc files should go
    configure:2852: $EMACS -batch -q -eval '(while load-path (princ (concat (car load-path) "\n")) (setq load-path (cdr load-path)))' </dev/null >conftest.out
    Loading 00debian-vars...
    Loading /etc/emacs/site-start.d/50a2ps.el (source)...
    Loading /etc/emacs/site-start.d/50autoconf.el (source)...
    Loading /etc/emacs/site-start.d/50cmake-data.el (source)...
    Loading /etc/emacs/site-start.d/50dictionaries-common.el (source)...
    Loading debian-ispell...
    Loading /var/cache/dictionaries-common/emacsen-ispell-default.el (source)...
    Loading /var/cache/dictionaries-common/emacsen-ispell-dicts.el (source)...
    Loading /etc/emacs/site-start.d/50psvn.el (source)...
    configure:2855: $? = 0
    configure:2868: result: ${datarootdir}/emacs/site-lisp
    configure:2881: checking for grep that handles long lines and -e
    configure:2939: result: /bin/grep
    configure:2944: checking for egrep
    configure:3006: result: /bin/grep -E
    configure:3011: checking for a sed that does not truncate output
    configure:3075: result: /bin/sed
    configure:3085: checking whether make is case sensitive
    configure:3100: result: yes
    configure:3279: creating ./config.status

    ## ---------------------- ##
    ## Running config.status. ##
    ## ---------------------- ##

    This file was extended by GNU Autoconf config.status 2.69, which was
    generated by GNU Autoconf 2.69.  Invocation command line was

      CONFIG_FILES    =
      CONFIG_HEADERS  =
      CONFIG_LINKS    =
      CONFIG_COMMANDS =
      $ ./config.status

    on cimepe36

    config.status:804: creating tests/Makefile
    config.status:804: creating tests/atlocal
    config.status:804: creating man/Makefile
    config.status:804: creating lib/emacs/Makefile
    config.status:804: creating Makefile
    config.status:804: creating doc/Makefile
    config.status:804: creating lib/Makefile
    config.status:804: creating lib/Autom4te/Makefile
    config.status:804: creating lib/autoscan/Makefile
    config.status:804: creating lib/m4sugar/Makefile
    config.status:804: creating lib/autoconf/Makefile
    config.status:804: creating lib/autotest/Makefile
    config.status:804: creating bin/Makefile
    config.status:1007: executing tests/atconfig commands
    configure:4386: WARNING: unrecognized options: --disable-silent-rules, --disable-dependency-tracking

    ## ---------------- ##
    ## Cache variables. ##
    ## ---------------- ##

    ac_cv_build=x86_64-pc-linux-gnu
    ac_cv_dir_trailing_space=yes
    ac_cv_env_EMACSLOADPATH_set=
    ac_cv_env_EMACSLOADPATH_value=
    ac_cv_env_EMACS_set=
    ac_cv_env_EMACS_value=
    ac_cv_env_M4_set=
    ac_cv_env_M4_value=
    ac_cv_env_build_alias_set=set
    ac_cv_env_build_alias_value=x86_64-linux
    ac_cv_env_host_alias_set=set
    ac_cv_env_host_alias_value=x86_64-linux
    ac_cv_env_target_alias_set=set
    ac_cv_env_target_alias_value=x86_64-linux
    ac_cv_host=x86_64-pc-linux-gnu
    ac_cv_path_EGREP='/bin/grep -E'
    ac_cv_path_EXPR=/usr/bin/expr
    ac_cv_path_GREP=/bin/grep
    ac_cv_path_M4=m4
    ac_cv_path_PERL=/usr/bin/perl
    ac_cv_path_SED=/bin/sed
    ac_cv_path_install='/usr/bin/install -c'
    ac_cv_path_mkdir=/bin/mkdir
    ac_cv_perl_flock_implemented=yes
    ac_cv_prog_AWK=gawk
    ac_cv_prog_EMACS=emacs
    ac_cv_prog_TEST_EMACS=emacs
    ac_cv_prog_emacs_ok=yes
    ac_cv_prog_gnu_m4_debugfile=--debugfile
    ac_cv_prog_gnu_m4_gnu=yes
    ac_cv_prog_make_make_case=yes
    ac_cv_prog_make_make_set=yes
    ac_cv_sh_n_works=no
    ac_cv_unsupported_fs_chars=
    am_cv_lispdir='${datarootdir}/emacs/site-lisp'

    ## ----------------- ##
    ## Output variables. ##
    ## ----------------- ##

    ACLOCAL='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run aclocal-1.11'
    AMTAR='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run tar'
    AUTOCONF='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run autoconf'
    AUTOHEADER='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run autoheader'
    AUTOMAKE='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run automake-1.11'
    AWK='gawk'
    CYGPATH_W='echo'
    DEFS='-DPACKAGE_NAME=\"GNU\ Autoconf\" -DPACKAGE_TARNAME=\"autoconf\" -DPACKAGE_VERSION=\"2.69\" -DPACKAGE_STRING=\"GNU\ Autoconf\ 2.69\" -DPACKAGE_BUGREPORT=\"bug-autoconf@gnu.org\" -DPACKAGE_URL=\"www.gnu.org/.../autoconf\" -DPACKAGE=\"autoconf\" -DVERSION=\"2.69\"'
    ECHO_C=''
    ECHO_N='-n'
    ECHO_T=''
    EGREP='/bin/grep -E'
    EMACS='emacs'
    EMACSLOADPATH=''
    EXPR='/usr/bin/expr'
    GREP='/bin/grep'
    HELP2MAN='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run help2man'
    INSTALL_DATA='${INSTALL} -m 644'
    INSTALL_PROGRAM='${INSTALL}'
    INSTALL_SCRIPT='${INSTALL}'
    INSTALL_STRIP_PROGRAM='$(install_sh) -c -s'
    LIBOBJS=''
    LIBS=''
    LTLIBOBJS=''
    M4='m4'
    M4_DEBUGFILE='--debugfile'
    M4_GNU='--gnu'
    MAKEINFO='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run makeinfo'
    MAKE_CASE_SENSITIVE_FALSE='#'
    MAKE_CASE_SENSITIVE_TRUE=''
    MKDIR_P='/bin/mkdir -p'
    PACKAGE='autoconf'
    PACKAGE_BUGREPORT='bug-autoconf@gnu.org'
    PACKAGE_NAME='GNU Autoconf'
    PACKAGE_STRING='GNU Autoconf 2.69'
    PACKAGE_TARNAME='autoconf'
    PACKAGE_URL='www.gnu.org/.../autoconf'
    PACKAGE_VERSION='2.69'
    PATH_SEPARATOR=':'
    PERL='/usr/bin/perl'
    PERL_FLOCK='yes'
    SED='/bin/sed'
    SET_MAKE=''
    SHELL='/bin/bash'
    STRIP='strip'
    TEST_EMACS='emacs'
    VERSION='2.69'
    ac_cv_dir_trailing_space='yes'
    ac_cv_sh_n_works='no'
    ac_cv_unsupported_fs_chars=''
    am__isrc=''
    am__leading_dot='.'
    am__tar='${AMTAR} chof - "$$tardir"'
    am__untar='${AMTAR} xf -'
    bindir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin'
    build='x86_64-pc-linux-gnu'
    build_alias='x86_64-linux'
    build_cpu='x86_64'
    build_os='linux-gnu'
    build_vendor='pc'
    datadir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share'
    datarootdir='${prefix}/share'
    docdir='${datarootdir}/doc/${PACKAGE_TARNAME}'
    dvidir='${docdir}'
    exec_prefix='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr'
    host='x86_64-pc-linux-gnu'
    host_alias='x86_64-linux'
    host_cpu='x86_64'
    host_os='linux-gnu'
    host_vendor='pc'
    htmldir='${docdir}'
    includedir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include'
    infodir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/info'
    install_sh='${SHELL} /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/install-sh'
    libdir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib'
    libexecdir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/lib/autoconf'
    lispdir='${datarootdir}/emacs/site-lisp'
    localedir='${datarootdir}/locale'
    localstatedir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/var'
    mandir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/share/man'
    mkdir_p='/bin/mkdir -p'
    oldincludedir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/include'
    pdfdir='${docdir}'
    prefix='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr'
    program_transform_name='s,x,x,'
    psdir='${docdir}'
    sbindir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin'
    sharedstatedir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/com'
    sysconfdir='/calcul/arago/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/etc'
    target_alias='x86_64-linux'

    ## ----------- ##
    ## confdefs.h. ##
    ## ----------- ##

    /* confdefs.h */
    #define PACKAGE_NAME "GNU Autoconf"
    #define PACKAGE_TARNAME "autoconf"
    #define PACKAGE_VERSION "2.69"
    #define PACKAGE_STRING "GNU Autoconf 2.69"
    #define PACKAGE_BUGREPORT "bug-autoconf@gnu.org"
    #define PACKAGE_URL "www.gnu.org/.../autoconf"
    #define PACKAGE "autoconf"
    #define VERSION "2.69"

    configure: exit 0
    ERROR: oe_runconf failed
    WARNING: exit code 1 from a shell command.
    ERROR: Function failed: do_configure (log file is located at /calcul/arago/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/autoconf-native/2.69-r11/temp/log.do_configure.12768)

  • Hi Michele,

    Please follow strictly the:
    www.arago-project.org/.../Setting_Up_Build_Environment
    Following all of these steps I builded it successfully.

    BR
    Ivan
  • Hi,

    Could you start in a new window and run:
    $ git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
    $ cd tisdk
    $ ./oe-layertool-setup.sh -f ./configs/amsdk/amsdk-06.00.00.00-config.txt
    $ cd build
    $ . conf/setenv
    $ export PATH=$HOME/arago-2011.09/armv5te/bin:$PATH
    $ MACHINE=am335x-evm TOOLCHAIN_BRAND=arago bitbake core-image-minimal
    If there are some errors please try with:
    $ MACHINE=am335x-evm TOOLCHAIN_BRAND=arago bitbake -v -p -e core-image-minimal

    And see in a logs if there are some errors.

    BR
    Ivan
  • Thanks ivan, looks like the error came from the Linaro toolchain being added at the end of PATH rather than at the beginning. The problem came up only when I asked for a new configuration, now everything is ok.
    Do you know if there are any information about setting up meta-arago inside Yocto?

    Regards,

    Michele