This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6467 network question



hi,friends,

I meet  the  following problem when I try to boot the DSP through the networks.could you give me some guides to make the net  ok from the following informations,thanks a lot in advance.

 

TI DaVinci EMAC: MAC address is 00:0e:99:02:b4:e9
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
Palm Chip BK3710 IDE Register Fail
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at c805c000 using DMA, IRQ 13
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50
2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
asoc: DIT <-> davinci-dit mapping ok
ALSA device list:
  #0: DaVinci DM6467 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests ..., OK
IP-Config: Got DHCP answer from 192.168.180.254, my address is 192.168.180.128
IP-Config: Complete:
      device=eth0, addr=192.168.180.128, mask=255.255.255.0, gw=255.255.255.255,

     host=192.168.180.128, domain=localdomain, nis-domain=(none),
     bootserver=192.168.180.254, rootserver=192.168.0.8, rootpath=
Looking up port of RPC 100003/2 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get mountd port number from server, using default
mount: RPC call returned error 101
Root-NFS: Server returned error -101 while mounting /home/jiang/workdir/filesys/

VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

Booting PSP Boot Loader

Starting NAND Copy

Booting Application @ 0x81080000


U-Boot 1.2.0 (May 20 2009 - 01:04:07)

I2C:   ready
DRAM:  256 MB
unknown vendor=0 Flash:  0 kB
NAND:  NAND device: Manufacturer ID: 0x20, Chip ID: 0xf1 (ST Micro NAND 128MiB 3
,3V 8-bit)
128 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 297MHz
Hit any key to stop autoboot:  0
TFTP from server 192.168.0.8; our IP address is 192.168.0.103
Filename 'uImage'.
Load address: 0x80700000
Loading: T T T T T T T #########################################################
########
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ################################################################
done
Bytes transferred = 1988128 (1e5620 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1988064 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
...................................................................... done, boo
ting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@localhost.localdomain)
(gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Wed
 Nov 25 11:27:39 EST 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM6467 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6467 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30720
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nf
sroot=192.168.0.8:/home/jiang/workdir/filesys/,nolock mem=120M davincihd_capture
.channel0_numbuffers=4
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 117504KB available (3401K code, 684K data, 172K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 48 gpio irqs
ch0 default output "COMPOSITE", mode "NTSC"
ch1 default output "", mode ""
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Nov 25 2009 11:23:17 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
CIR device registered successfully (Major = 252, Minor = 0)
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a ST16654

serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfec20400 (irq = 41) is a ST16650
V2
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ4
2): -28
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is 00:0e:99:02:b4:e9
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
Palm Chip BK3710 IDE Register Fail
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at c805c000 using DMA, IRQ 13
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50
2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
asoc: DIT <-> davinci-dit mapping ok
ALSA device list:
  #0: DaVinci DM6467 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 192.168.180.254, my address is 192.168.180.128
IP-Config: Complete:
      device=eth0, addr=192.168.180.128, mask=255.255.255.0, gw=255.255.255.255,

     host=192.168.180.128, domain=localdomain, nis-domain=(none),
     bootserver=192.168.180.254, rootserver=192.168.0.8, rootpath=
Looking up port of RPC 100003/2 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get mountd port number from server, using default
mount: RPC call returned error 101
Root-NFS: Server returned error -101 while mounting /home/jiang/workdir/filesys/

VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
128 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 297MHz
Hit any key to stop autoboot:  0
TFTP from server 192.168.0.8; our IP address is 192.168.0.103
Filename 'uImage'.
Load address: 0x80700000
Loading: T T T T T T ###########################################################
######
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ################################################################
done
Bytes transferred = 1988128 (1e5620 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1988064 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
...................................................................... done, boo
ting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@localhost.localdomain)
(gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Wed
 Nov 25 11:27:39 EST 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM6467 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6467 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30720
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nf
sroot=192.168.0.8:/home/jiang/workdir/filesys/,nolock mem=120M davincihd_capture
.channel0_numbuffers=4
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 117504KB available (3401K code, 684K data, 172K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 48 gpio irqs
ch0 default output "COMPOSITE", mode "NTSC"
ch1 default output "", mode ""
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Nov 25 2009 11:23:17 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
CIR device registered successfully (Major = 252, Minor = 0)
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a ST16654

serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfec20400 (irq = 41) is a ST16650
V2
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ4
2): -28
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is 00:0e:99:02:b4:e9
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
Palm Chip BK3710 IDE Register Fail
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at c805c000 using DMA, IRQ 13
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50
2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
asoc: DIT <-> davinci-dit mapping ok
ALSA device list:
  #0: DaVinci DM6467 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 192.168.180.254, my address is 192.168.180.128
IP-Config: Complete:
      device=eth0, addr=192.168.180.128, mask=255.255.255.0, gw=255.255.255.255,

     host=192.168.180.128, domain=localdomain, nis-domain=(none),
     bootserver=192.168.180.254, rootserver=192.168.0.8, rootpath=
Looking up port of RPC 100003/2 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get mountd port number from server, using default
mount: RPC call returned error 101
Root-NFS: Server returned error -101 while mounting /home/jiang/workdir/filesys/

VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
 0
TFTP from server 192.168.0.8; our IP address is 192.168.0.103
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ################################################################
done
Bytes transferred = 1988128 (1e5620 hex)
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1988064 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
...................................................................... done, boo
ting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@localhost.localdomain)
(gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Wed
 Nov 25 11:27:39 EST 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM6467 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6467 variant 0x0
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 30720
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nf
sroot=192.168.0.8:/home/jiang/workdir/filesys/,nolock mem=120M davincihd_capture
.channel0_numbuffers=4
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 117504KB available (3401K code, 684K data, 172K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 48 gpio irqs
ch0 default output "COMPOSITE", mode "NTSC"
ch1 default output "", mode ""
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Nov 25 2009 11:23:17 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
CIR device registered successfully (Major = 252, Minor = 0)
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a ST16654

serial8250.0: ttyS1 at MMIO map 0x1c20400 mem 0xfec20400 (irq = 41) is a ST16650
V2
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ4
2): -28
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is 00:0e:99:02:b4:e9
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized ATAEN
    ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
Palm Chip BK3710 IDE Register Fail
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc: USB Host mode controller at c805c000 using DMA, IRQ 13
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50
2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
asoc: DIT <-> davinci-dit mapping ok
ALSA device list:
  #0: DaVinci DM6467 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests ..., OK
IP-Config: Got DHCP answer from 192.168.180.254, my address is 192.168.180.128
IP-Config: Complete:
      device=eth0, addr=192.168.180.128, mask=255.255.255.0, gw=255.255.255.255,

     host=192.168.180.128, domain=localdomain, nis-domain=(none),
     bootserver=192.168.180.254, rootserver=192.168.0.8, rootpath=
Looking up port of RPC 100003/2 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.0.8
portmap: RPC call returned error 101
Root-NFS: Unable to get mountd port number from server, using default
mount: RPC call returned error 101
Root-NFS: Server returned error -101 while mounting /home/jiang/workdir/filesys/

VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

  • Hi Wenhao Xu,


    Can you provide the "bootargs" here. Seems to be some problem with accessing the NFS filesystem which are you are trying to mount.


    Regards,
    Sid

  • Hi,Sid,

    Thanks for your answer firstly,the following information includes the "bootargs",could you give me some suggestions  to solve the above problem?

    DM6467 HD EVM # printenv
    bootdelay=4
    baudrate=115200
    filesize=1e5674
    fileaddr=80700000
    ipaddr=192.168.0.103
    bootcmd=tftp;bootm
    serverip=192.168.0.8
    bootfile=uImage
    rootpath=/home/jiang/workdir/filesys/
    nfshost=192.168.0.8
    stdin=serial
    stdout=serial
    stderr=serial
    ethaddr=00:0e:99:02:b4:e9
    bootargs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.16
    8.0.8:/home/jiang/workdir/filesys/,nolock mem=120M davincihd_capture.channel0_nu
    mbuffers=4

    Best regards,

            Wenhao Xu

     

  • Hi Wenhao,

    "Looking up port of RPC 100003/2 on 192.168.0.8
    portmap: RPC call returned error 101
    Root-NFS: Unable to get nfsd port number from server, using default
    Looking up port of RPC 100005/1 on 192.168.0.8"

    This indicates that the kernel is somehow unable to detect connection over ethernet using the present IP. This may require a little more debugging.

    Can you put in two commands namely "dhcp" (ethernet config) and "minicom" (serial config) and post the output here? It may point out the problme.

    If dhcp gives out faulty output, then probably dhcp hasnt been configured properly. As an alternative, you could go for a static IP and try out the same.

    Post the results for the same.

    Hope this helps.

    Regards,

    Sid