This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Play Wave File In LCDK L138 using Staterware OS

Other Parts Discussed in Thread: OMAPL138

Play Wave File In LCDK L138 using Staterware OS    any Example Code

  • Hi,

    Thanks for your post.

    You could download the latest release of StarterWare for OMAPL138 from the below URL:

    http://software-dl.ti.com/dsps/dsps_public_sw/c6000/starterware/01_10/index_FDS.html

    For Starterware McASP configuration programming, you could refer the below wiki:

    http://processors.wiki.ti.com/index.php/StarterWare_McASP

    The McASP starterware audio loopback example demonstrates audio input and output in I2S mode using DMA. The audio input on the LINE IN is looped back to the audio ouput on LINE OUT of the EVM. Before running the application, connect an audio source to the LINE IN connector and speakers or headphones to the LINE OUT connector. While the application runs, audio is piped from LINE IN to LINE OUT

    http://processors.wiki.ti.com/index.php/StarterWare_Audio_Application

    After installing the latest starterware for OMAPL138 LCDK, you could see the McASP audio loopback example .CCS project at the below path:

    ~\ti\OMAPL138_StarterWare_1_10_04_01\build\c674x\cgt_ccs\omapl138\lcdkOMAPL138\mcasp

    and the source for the above project could be found at the below path:

    ~\ti\OMAPL138_StarterWare_1_10_04_01\examples\lcdkOMAPL138\mcasp

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question

    -------------------------------------------------------------------------------------------------------