This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

change default ecc to Hamming ecc

Guru 20755 points

Hello,

I use DM8148, and wanted to use jffs2, which requires to change the default ecc from BCH8 ->HAMMING HW.

I made modifications in both kernel and u-boot:

And also verified that I program everything with:

nandecc hw 0.

 But the 1st stage u-boot does not start (there is no printing at all after reset)

I would like to ask if I there is some additional step I need to do.

How does the flash nand knows after reset that it needs to read from address 0, with hamming ecc ?

Thanks you,

Ran

  • Ran,

    In DVR RDK 2.80.xx.xx release, PSP used has ECC as BCH8 which is incompatible with jffs2. There are several flashing / run time issues observed due to this incompatibility.

    There are 2 solutions
    - Migrate to UBIFS
    - For customers wanting to use jffs2, we are providing patches / instructions to roll back to ECC mechanism to 1Bit ECC <which was present in older PSP releases>. With these patches jffs2 should work properly.

    You should reverse (pull out) all the BCH8 related patches from DVR RDK PSP (u-boot and kernel). Or contact your local TI FAE for access to:

    Refer this document for details - DM81xx_DVR_RDK_NAND_ECC_App_Notes.pdf
    Patches - 1BitECC_LSP_Patches.tar.gz

    Regards,
    Pavel
  • Hi Pavel,

    Thanks for the reply.
    According to the foolwing link it seems that Hamming (is it same as "1Bit ECC " you refers to ?) is not advised for jffs2:
    e2e.ti.com/.../239237
    So I'm not sure now if it is advised or not to get back to Hamming. What do you think ?

    Do you know where I can find the patches for kernel/u-boot for reversing to Hamming ?

    Regards,
    Ran
  • Ran,

    Ran Shalit said:
    Hamming (is it same as "1Bit ECC " you refers to ?)

    Yes, Hamming ECC is 1bit ECC.

    Ran Shalit said:
    According to the foolwing link it seems that Hamming (is it same as "1Bit ECC " you refers to ?) is not advised for jffs2:

    I checked this e2e thread, I can not find such advice! I can even find the reverse - there is advice for using Hamming (1-bit ECC) for jffs2. Can you point which post exactly (from this e2e thread) advice that we should not use jffs2 with Hamming?

    Ran Shalit said:
    Do you know where I can find the patches for kernel/u-boot for reversing to Hamming ?

    In the below link (accessible only through local FAE/TI representative):

    Regards,
    Pavel

  • Hi Pavel,

    I probably missed something.
    In the thread it is said: "These 'uncorrectable' ECC errors should be the real issue causing you kernel to panic. HAM1 (Hamming code) can 'detect upto 2-bit-flips errors, but correct only 1-bit-flip errors' So somewhere your NAND is seeing multi-bit-flip errors."
    I'm afraid that I might get the same errors if I reverse to Hamming.

    Regards,
    Ran
  • Ran,

    Ran Shalit said:
    In the thread it is said: "These 'uncorrectable' ECC errors should be the real issue causing you kernel to panic. HAM1 (Hamming code) can 'detect upto 2-bit-flips errors, but correct only 1-bit-flip errors' So somewhere your NAND is seeing multi-bit-flip errors."

    I do not see recommendation to use BCH8 with JFFS2 in the above quoted text. This is the below e2e post from Pekon:

    Reading this post, I do not see recommendation to use JFFS2 with BCH8. I see these 2 recommendations:

    (a) Move to UBIFS File-system. (preferred)  - this means using BCH8 with UBIFS

    (b) Use a NAND device which has more OOB(spare) bytes per page of NAND (like 4K/224B NAND). - this means use Hamming with JFFS2, but with other type of NAND chip

    Regards,
    Pavel

  • Hi Pavel,

    Thank you very much for the time and clarifications of this issue.

    Best Regards,
    Ran
  • Hi Pavel,

    I hope you can assist me more with this issue.

    I am still waiting for the internal patch from FAE (is the patch relevant for u-boot or only linux ?) ,

    But I have already started to make changes according to :

    ;a=commitdiff;h=fb8b435ea1745edbbb78c64e5f87c27169d33f9b;hp=c97321728537e4af572e4420b3c05167dad4931e

    and u-boot 1st stage already get stack. This is the sequence I'm doing:

    1. made changes in u-boot 1st stage according to patch above inorder to use Hamming code.

    2. nand scrub

    3. program the compiled 1st stage u-boot into nand with ecc hw 0 (nandecc hw 0)

    4. reset board.

    TI8148_EVM#run rf_xl_new; run rf_ub_new

    NAND erase: device 0 offset 0x0, size 0x20000
    Erasing at 0x0 -- 100% complete.
    OK
    link up on port 0, speed 100, full duplex
    Using cpsw device
    TFTP from server 10.0.0.1; our IP address is 10.0.0.2
    Filename 'u-boot.min.nand'.
    Load address: 0x81000000
    Loading: T ######################
    done
    Bytes transferred = 110128 (0x1ae30)
    HW ECC Hamming Code selected

    NAND write: device 0 offset 0x0, size 0x20000
    131072 bytes written: OK

    TI8148_EVM#reset

    resetting ...

    <<----- nothing get printed after reset

    Attached ti81xx_nand.c with changes for Hamming:

    /*
     * (C) Copyright 2004-2008 Texas Instruments, <www.ti.com>
     * Mansoor Ahamed <mansoor.ahamed@ti.com>
     *
     * Derived from work done by Rohit Choraria <rohitkc@ti.com> for omap
     *
     * See file CREDITS for list of people who contributed to this
     * project.
     *
     * This program is free software; you can redistribute it and/or
     * modify it under the terms of the GNU General Public License as
     * published by the Free Software Foundation; either version 2 of
     * the License, or (at your option) any later version.
     *
     * This program is distributed in the hope that it will be useful,
     * but WITHOUT ANY WARRANTY; without even the implied warranty of
     * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
     * GNU General Public License for more details.
     *
     * You should have received a copy of the GNU General Public License
     * along with this program; if not, write to the Free Software
     * Foundation, Inc., 59 Temple Place, Suite 330, Boston,
     * MA 02111-1307 USA
     */
    
    #include <common.h>
    #include <asm/io.h>
    #include <asm/errno.h>
    #include <asm/arch/cpu.h>
    #include <asm/arch/mem.h>
    #include <asm/arch/nand.h>
    #include <linux/mtd/nand_ecc.h>
    #include <nand.h>
    
    struct nand_bch_priv {
    	uint8_t mode;
    	uint8_t type;
    	uint8_t nibbles;
    };
    
    /* bch types */
    #define ECC_BCH4	0
    #define ECC_BCH8	1
    #define ECC_BCH16	2
    
    /* BCH nibbles for diff bch levels */
    #define NAND_ECC_HW_BCH ((uint8_t)(NAND_ECC_HW_OOB_FIRST) + 1)
    #define ECC_BCH4_NIBBLES	13
    #define ECC_BCH8_NIBBLES	26
    #define ECC_BCH16_NIBBLES	52
    
    static uint8_t cs;
    
    static struct nand_ecclayout hw_nand_oob = GPMC_NAND_HW_ECC_LAYOUT_KERNEL;
    #ifdef CONFIG_UD8168_DVR
    static struct nand_ecclayout hw_nand_oob_p4k = GPMC_NAND_HW_ECC_LAYOUT_KERNEL_PG4K;
    #endif
    static struct nand_ecclayout hw_bch4_nand_oob = GPMC_NAND_HW_BCH4_ECC_LAYOUT;
    static struct nand_ecclayout hw_bch8_nand_oob = GPMC_NAND_HW_BCH8_ECC_LAYOUT;
    static struct nand_ecclayout hw_bch16_nand_oob = GPMC_NAND_HW_BCH16_ECC_LAYOUT;
    
    #ifdef CONFIG_UD8168_DVR
    extern int dvr_get_hw_version(void);
    #endif
    
    static struct nand_bch_priv bch_priv = {
    	.mode = NAND_ECC_HW_BCH,
    	.type = ECC_BCH8,
    	.nibbles = ECC_BCH8_NIBBLES
    };
    
    /*
     * ti81xx_read_bch8_result - Read BCH result for BCH8 level
     *
     * @mtd:	MTD device structure
     * @big_endian:	When set read register 3 first
     * @ecc_code:	Read syndrome from BCH result registers
     */
    static void ti81xx_read_bch8_result(struct mtd_info *mtd, uint8_t big_endian,
    				uint8_t *ecc_code)
    {
    	uint32_t *ptr;
    	int8_t i = 0, j;
    
    	if (big_endian) {
    		ptr = &gpmc_cfg->bch_result_0_3[0].bch_result_x[3];
    		ecc_code[i++] = readl(ptr) & 0xFF;
    		ptr--;
    		for (j = 0; j < 3; j++) {
    			ecc_code[i++] = (readl(ptr) >> 24) & 0xFF;
    			ecc_code[i++] = (readl(ptr) >> 16) & 0xFF;
    			ecc_code[i++] = (readl(ptr) >>  8) & 0xFF;
    			ecc_code[i++] = readl(ptr) & 0xFF;
    			ptr--;
    		}
    	}
    	else {
    		ptr = &gpmc_cfg->bch_result_0_3[0].bch_result_x[0];
    		for (j = 0; j < 3; j++) {
    			ecc_code[i++] = readl(ptr) & 0xFF;
    			ecc_code[i++] = (readl(ptr) >>  8) & 0xFF;
    			ecc_code[i++] = (readl(ptr) >> 16) & 0xFF;
    			ecc_code[i++] = (readl(ptr) >> 24) & 0xFF;
    			ptr++;
    		}
    		ecc_code[i++] = readl(ptr) & 0xFF;
    	}
    }
    
    /*
     * ti81xx_ecc_disable - Disable H/W ECC calculation
     *
     * @mtd:	MTD device structure
     *
     */
    static void ti81xx_ecc_disable(struct mtd_info *mtd) {
    
    	writel((readl(&gpmc_cfg->ecc_config) & ~0x1),
    		&gpmc_cfg->ecc_config);
    }
    
    #if 0
    /*
     * ti81xx_ecc_enable_bch - Enable BCH H/W ECC calculation
     *
     * @mtd:	MTD device structure
     *
     */
    static void ti81xx_ecc_enable_bch(struct mtd_info *mtd) {
    	uint32_t val;
    
    	val = readl(&gpmc_cfg->ecc_control);
    	val |= 0x00000100u;
    	writel(val, &gpmc_cfg->ecc_control); /* clear ECC outputs */
    
    	val = readl(&gpmc_cfg->ecc_control);
    	val &= ~0xF;
    	val |= 0x1;
    	writel(val, &gpmc_cfg->ecc_control);  /* reset ecc pointer to result 1 */
    
    	val = readl(&gpmc_cfg->ecc_config);
    	val |= 0x1;
    	writel(val, &gpmc_cfg->ecc_config); /* enable ecc */
    }
    #endif
    
    /*
     * ti81xx_nand_hwcontrol - Set the address pointers correctly for the
     *			following address/data/command operation
     */
    static void ti81xx_nand_hwcontrol(struct mtd_info *mtd, int32_t cmd,
    				uint32_t ctrl)
    {
    	register struct nand_chip *this = mtd->priv;
    
    	/*
    	 * Point the IO_ADDR to DATA and ADDRESS registers instead
    	 * of chip address
    	 */
    	switch (ctrl) {
    	case NAND_CTRL_CHANGE | NAND_CTRL_CLE:
    		this->IO_ADDR_W = (void __iomem *)&gpmc_cfg->cs[cs].nand_cmd;
    		break;
    	case NAND_CTRL_CHANGE | NAND_CTRL_ALE:
    		this->IO_ADDR_W = (void __iomem *)&gpmc_cfg->cs[cs].nand_adr;
    		break;
    	case NAND_CTRL_CHANGE | NAND_NCE:
    		this->IO_ADDR_W = (void __iomem *)&gpmc_cfg->cs[cs].nand_dat;
    		break;
    	}
    
    	if (cmd != NAND_CMD_NONE)
    		writeb(cmd, this->IO_ADDR_W);
    }
    
    /*
     * ti81xx_hwecc_init_bch - Initialize the BCH Hardware ECC for NAND flash in
     * 				GPMC controller
     * @mtd:       MTD device structure
     * @mode:	Read/Write mode
     */
    static void ti81xx_hwecc_init_bch(struct nand_chip *chip, int32_t mode)
    {
    	uint32_t val, dev_width = (chip->options & NAND_BUSWIDTH_16) >> 1;
    	uint32_t unused_length = 0;
    	struct nand_bch_priv *bch = chip->priv;
    
    	switch(bch->nibbles) {
    		case ECC_BCH4_NIBBLES:
    			unused_length = 3;
    			break;
    		case ECC_BCH8_NIBBLES:
    			unused_length = 2;
    			break;
    		case ECC_BCH16_NIBBLES:
    			unused_length = 0;
    			break;
    	}
    
    	/* Clear the ecc result registers, select ecc reg as 1 */
    	writel(ECCCLEAR | ECCRESULTREG1, &gpmc_cfg->ecc_control);
    
    	switch (mode) {
    		case NAND_ECC_WRITE:
    			/* eccsize1 config */
    			val = ((unused_length + bch->nibbles) << 22);
    			break;
    
    		case NAND_ECC_READ:
    		default:
    			/* by default eccsize0 selected for ecc1resultsize */
    			/* eccsize0 config */
    			val  = (bch->nibbles << 12);
    			/* eccsize1 config */
    			val |= (unused_length << 22);
    			break;
    	}
    	/* ecc size configuration */
    	writel(val, &gpmc_cfg->ecc_size_config);
    	/* by default 512bytes sector page is selected */
    	/* set bch mode */
    	val  = (1 << 16);
    	/* bch4 / bch8 / bch16 */
    	val |= (bch->type << 12);
    	/* set wrap mode to 1 */
    	val |= (1 << 8);
    	val |= (dev_width << 7);
    	val |= (cs << 1);
    	/* enable ecc */
    	/* val |= (1); */ /* should not enable ECC just init i.e. config */
    	writel(val, &gpmc_cfg->ecc_config);
    }
    
    
    /*
     * ti81xx_hwecc_init - Initialize the Hardware ECC for NAND flash in
     *                   GPMC controller
     * @mtd:        MTD device structure
     *
     */
    static void ti81xx_hwecc_init(struct nand_chip *chip)
    {
    	/*
    	 * Init ECC Control Register
    	 * Clear all ECC | Enable Reg1
    	 */
    	writel(ECCCLEAR | ECCRESULTREG1, &gpmc_cfg->ecc_control);
    	writel(ECCSIZE1 | ECCSIZE0 | ECCSIZE0SEL, &gpmc_cfg->ecc_size_config);
    }
    
    /*
     * gen_true_ecc - This function will generate true ECC value, which
     * can be used when correcting data read from NAND flash memory core
     *
     * @ecc_buf:	buffer to store ecc code
     *
     * @return:	re-formatted ECC value
     */
    static uint32_t gen_true_ecc(uint8_t *ecc_buf)
    {
    	return ecc_buf[0] | (ecc_buf[1] << 16) | ((ecc_buf[2] & 0xF0) << 20) |
    		((ecc_buf[2] & 0x0F) << 8);
    }
    
    /*
     * ti81xx_rotate_ecc_bch - Rotate the syndrome bytes
     *
     * @mtd:	MTD device structure
     * @calc_ecc:	ECC read from ECC registers
     * @syndrome:	Rotated syndrome will be retuned in this array
     *
     */
    static void ti81xx_rotate_ecc_bch(struct mtd_info *mtd, uint8_t *calc_ecc,
    		uint8_t *syndrome)
    {
    	struct nand_chip *chip = mtd->priv;
    	struct nand_bch_priv *bch = chip->priv;
    	uint8_t n_bytes = 0;
    	int8_t i,j;
    
    	switch(bch->type) {
    		case ECC_BCH4:
    			n_bytes = 8;
    			break;
    
    		case ECC_BCH16:
    			n_bytes = 28;
    			break;
    
    		case ECC_BCH8:
    		default:
    			n_bytes = 13;
    			break;
    	}
    
    	for (i = 0, j = (n_bytes-1); i < n_bytes; i++, j--)
    		syndrome[i] =  calc_ecc[j];
    }
    
    
    /*
     * ti81xx_fix_errors_bch - Correct bch error in the data
     *
     * @mtd:	MTD device structure
     * @data:	Data read from flash
     * @error_count:Number of errors in data
     * @error_loc:	Locations of errors in the data
     *
     */
    static void ti81xx_fix_errors_bch(struct mtd_info *mtd, uint8_t *data,
    		uint32_t error_count, uint32_t *error_loc)
    {
    	struct nand_chip *chip = mtd->priv;
    	struct nand_bch_priv *bch = chip->priv;
    	uint8_t count = 0;
    	uint32_t error_byte_pos;
    	uint32_t error_bit_mask;
    	uint32_t last_bit = (bch->nibbles * 4) - 1;
    
    	/* Flip all bits as specified by the error location array. */
    	/* FOR( each found error location flip the bit ) */
    	for (count = 0; count < error_count; count++) {
    		if (error_loc[count] > last_bit) {
    			/* Remove the ECC spare bits from correction. */
    			error_loc[count] -= (last_bit + 1);
    			/* Offset bit in data region */
    			error_byte_pos = ((512 * 8) - (error_loc[count]) - 1) /8;
    			/* Error Bit mask */
    			error_bit_mask = 0x1 << (error_loc[count] % 8);
    			/* Toggle the error bit to make the correction. */
    			data[error_byte_pos] ^= error_bit_mask;
    		}
    	}
    }
    
    /*
     * ti81xx_correct_data_bch - Compares the ecc read from nand spare area
     * with ECC registers values and corrects one bit error if it has occured
     *
     * @mtd:	MTD device structure
     * @dat:	page data
     * @read_ecc:	ecc read from nand flash (ignored)
     * @calc_ecc:	ecc read from ECC registers
     *
     * @return 0 if data is OK or corrected, else returns -1
     */
    static int ti81xx_correct_data_bch(struct mtd_info *mtd, uint8_t *dat,
    				uint8_t *read_ecc, uint8_t *calc_ecc)
    {
    	struct nand_chip *chip = mtd->priv;
    	struct nand_bch_priv *bch = chip->priv;
    	uint8_t syndrome[28];
    	uint32_t error_count = 0;
    	uint32_t error_loc[8];
    //ranran ecc
    #if 0
    	/* erased page detection.  An erased page
    	 * has the following syndromes and all
    	 * OOB bytes are 0xFF */
    	uint8_t erased_syndromes[13] = {
    		0x7B, 0x99, 0xFF, 0x6B,
    		0xAC, 0xCC, 0xBE, 0xD2,
    		0x8B, 0x16, 0x14, 0xDB,
    		0xF3
    	};
    	unsigned int erased;
    	uint8_t i;
    #endif
    	elm_reset();
    	elm_config((enum bch_level)(bch->type));
    
    	/* while reading ECC result we read it in big endian.
    	 * Hence while loading to ELM we have rotate to get the right endian.
    	 */
    	ti81xx_rotate_ecc_bch(mtd, calc_ecc, syndrome);
    
    #ifdef NAND_DEBUG
    	{
    		printf("----\necc\n---\n");
    		for (i = 0; i < 13; i++)
    			printf("  0x%2x", syndrome[i]);
    		printf("\n");
    	}
    #endif
    
    	/* use elm module to check for errors */
    	if (elm_check_error(syndrome, bch->nibbles, &error_count, error_loc) != 0) {
                //ranran ecc - add 2 lines
    #if 1
                        printf("ECC: uncorrectable.\n");
                        return -1;
                    }
    #else
    		/* was this an erased page?
    		 * Check syndromes and OOB bytes */
    		erased = 1;
    		for (i = 0; i < 13; i++) {
    			if ((chip->oob_poi[i] != 0xFF) ||
    					(syndrome[i] != erased_syndromes[i])) {
    				erased = 0;
    				break;
    			}
    		}
    		if (!erased) {
    			printf("ECC: uncorrectable.\n");
    			return -1;
    		}
    		error_count = 0;
    	}
    #endif
    	/* correct bch error */
    	if (error_count > 0) {
    		ti81xx_fix_errors_bch(mtd, dat, error_count, error_loc);
    	}
    
    	return 0;
    }
    
    
    /*
     * ti81xx_correct_data - Compares the ecc read from nand spare area with ECC
     * registers values and corrects one bit error if it has occured
     * Further details can be had from TI81xx TRM and the following selected links:
     * http://en.wikipedia.org/wiki/Hamming_code
     * http://www.cs.utexas.edu/users/plaxton/c/337/05f/slides/ErrorCorrection-4.pdf
     *
     * @mtd:		 MTD device structure
     * @dat:		 page data
     * @read_ecc:		 ecc read from nand flash
     * @calc_ecc:		 ecc read from ECC registers
     *
     * @return 0 if data is OK or corrected, else returns -1
     */
    static int ti81xx_correct_data(struct mtd_info *mtd, uint8_t *dat,
    				uint8_t *read_ecc, uint8_t *calc_ecc)
    {
    	uint32_t orig_ecc, new_ecc, res, hm;
    	uint16_t parity_bits, byte;
    	uint8_t bit;
    
    	/* Regenerate the orginal ECC */
    	orig_ecc = gen_true_ecc(read_ecc);
    	new_ecc = gen_true_ecc(calc_ecc);
    	/* Get the XOR of real ecc */
    	res = orig_ecc ^ new_ecc;
    	if (res) {
    		/* Get the hamming width */
    		hm = hweight32(res);
    		/* Single bit errors can be corrected! */
    		if (hm == 12) {
    			/* Correctable data! */
    			parity_bits = res >> 16;
    			bit = (parity_bits & 0x7);
    			byte = (parity_bits >> 3) & 0x1FF;
    			/* Flip the bit to correct */
    			dat[byte] ^= (0x1 << bit);
    		} else if (hm == 1) {
    			printf("Error: Ecc is wrong\n");
    			/* ECC itself is corrupted */
    			return 2;
    		} else {
    			/*
    			 * hm distance != parity pairs OR one, could mean 2 bit
    			 * error OR potentially be on a blank page..
    			 * orig_ecc: contains spare area data from nand flash.
    			 * new_ecc: generated ecc while reading data area.
    			 * Note: if the ecc = 0, all data bits from which it was
    			 * generated are 0xFF.
    			 * The 3 byte(24 bits) ecc is generated per 512byte
    			 * chunk of a page. If orig_ecc(from spare area)
    			 * is 0xFF && new_ecc(computed now from data area)=0x0,
    			 * this means that data area is 0xFF and spare area is
    			 * 0xFF. A sure sign of a erased page!
    			 */
    			if ((orig_ecc == 0x0FFF0FFF) && (new_ecc == 0x00000000))
    				return 0;
    			printf("Error: Bad compare! failed\n");
    			/* detected 2 bit error */
    			return -1;
    		}
    	}
    	return 0;
    }
    
    /*
     *  ti81xx_calculate_ecc_bch - Read BCH ECC result
     *
     *  @mtd:	MTD structure
     *  @dat:	unused
     *  @ecc_code:	ecc_code buffer
     */
    static int ti81xx_calculate_ecc_bch(struct mtd_info *mtd, const uint8_t *dat,
    				uint8_t *ecc_code)
    {
    	struct nand_chip *chip = mtd->priv;
    	struct nand_bch_priv *bch = chip->priv;
    	uint8_t big_endian = 1;
    	int8_t ret = 0;
    
    	if (bch->type == ECC_BCH8)
    		ti81xx_read_bch8_result(mtd, big_endian, ecc_code);
    	else /* BCH4 and BCH16 currently not supported */
    		ret = -1;
    
    #ifdef NAND_DEBUG
    	{
    		int8_t i = 0;
    		printf("----\nECC\n---\n");
    		for (i = 0; i < 13; i++)
    			printf("  0x%2x", ecc_code[i]);
    		printf("\n");
    	}
    #endif
    
    	/*
    	 * Stop reading anymore ECC vals and clear old results
    	 * enable will be called if more reads are required
    	 */
    	ti81xx_ecc_disable(mtd);
    
    	return ret;
    }
    
    
    /*
     *  ti81xx_calculate_ecc - Generate non-inverted ECC bytes.
     *
     *  Using noninverted ECC can be considered ugly since writing a blank
     *  page ie. padding will clear the ECC bytes. This is no problem as
     *  long nobody is trying to write data on the seemingly unused page.
     *  Reading an erased page will produce an ECC mismatch between
     *  generated and read ECC bytes that has to be dealt with separately.
     *  E.g. if page is 0xFF (fresh erased), and if HW ECC engine within GPMC
     *  is used, the result of read will be 0x0 while the ECC offsets of the
     *  spare area will be 0xFF which will result in an ECC mismatch.
     *  @mtd:	MTD structure
     *  @dat:	unused
     *  @ecc_code:	ecc_code buffer
     */
    static int ti81xx_calculate_ecc(struct mtd_info *mtd, const uint8_t *dat,
    				uint8_t *ecc_code)
    {
    	u_int32_t val;
    
    	/* Start Reading from HW ECC1_Result = 0x200 */
    	val = readl(&gpmc_cfg->ecc1_result);
    
    	ecc_code[0] = val & 0xFF;
    	ecc_code[1] = (val >> 16) & 0xFF;
    	ecc_code[2] = ((val >> 8) & 0x0F) | ((val >> 20) & 0xF0);
    
    	/*
    	 * Stop reading anymore ECC vals and clear old results
    	 * enable will be called if more reads are required
    	 */
    	writel(0x000, &gpmc_cfg->ecc_config);
    
    	return 0;
    }
    
    /**
     * ti81xx_write_page_bch - [REPLACABLE] hardware ecc based page write function
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @buf:	data buffer
     */
    static void ti81xx_write_page_bch(struct mtd_info *mtd,
    	struct nand_chip *chip, const uint8_t *buf)
    {
    	int i, eccsize = chip->ecc.size;
    	int eccbytes = chip->ecc.bytes;
    	int eccsteps = chip->ecc.steps;
    	uint8_t *ecc_calc = chip->buffers->ecccalc;
    	const uint8_t *p = buf;
    	uint32_t *eccpos = chip->ecc.layout->eccpos;
    
    	for (i = 0; eccsteps; eccsteps--, i += eccbytes, p += eccsize) {
    		chip->ecc.hwctl(mtd, NAND_ECC_WRITE);
    		chip->write_buf(mtd, p, eccsize);
    		chip->ecc.calculate(mtd, p, &ecc_calc[i]);
    	}
    
    	for (i = 0; i < chip->ecc.total; i++)
    		chip->oob_poi[eccpos[i]] = ecc_calc[i];
    
    	chip->write_buf(mtd, chip->oob_poi, mtd->oobsize);
    }
    
    
    /**
     * ti81xx_read_page_bch - hardware ecc based page read function
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @buf:	buffer to store read data
     * @page:	page number to read
     *
     */
    static int ti81xx_read_page_bch(struct mtd_info *mtd, struct nand_chip *chip,
    				uint8_t *buf, int page)
    {
    	int i, eccsize = chip->ecc.size;
    	int eccbytes = chip->ecc.bytes;
    	int eccsteps = chip->ecc.steps;
    	uint8_t *p = buf;
    	uint8_t *ecc_calc = chip->buffers->ecccalc;
    	uint8_t *ecc_code = chip->buffers->ecccode;
    	uint32_t *eccpos = chip->ecc.layout->eccpos;
    	uint8_t *oob = chip->oob_poi;
    	uint32_t data_pos;
    	uint32_t oob_pos;
    
    	data_pos = 0;
    	/* oob area start */
    	oob_pos = (eccsize * eccsteps) + chip->ecc.layout->eccpos[0];
    	//oob_pos = (eccsize * eccsteps) + 2;
    
    	for (i = 0; eccsteps; eccsteps--, i += eccbytes, p += eccsize,
    				oob += eccbytes) {
    		chip->ecc.hwctl(mtd, NAND_ECC_READ);
    		/* read data */
    		chip->cmdfunc(mtd, NAND_CMD_RNDOUT, data_pos, page);
    		chip->read_buf(mtd, p, eccsize);
    #ifdef NAND_DEBUG
    		{
    			uint32_t j;
    			printf("----\nDATA\n---\n");
    			for (j = 0; j < 13; j++)
    				printf("  0x%2x", p[j]);
    			printf("\n");
    		}
    #endif
    
    		/* read respective ecc from oob area */
    		chip->cmdfunc(mtd, NAND_CMD_RNDOUT, oob_pos, page);
    		chip->read_buf(mtd, oob, eccbytes);
    #ifdef NAND_DEBUG
    		{
    			uint32_t j;
    			printf("----\nOOB\n---\n");
    			for (j = 0; j < 13; j++)
    				printf("  0x%2x", oob[j]);
    			printf("\n");
    		}
    #endif
    		/* read syndrome */
    		chip->ecc.calculate(mtd, p, &ecc_calc[i]);
    
    		data_pos += eccsize;
    		oob_pos += eccbytes;
    	}
    
    	for (i = 0; i < chip->ecc.total; i++)
    		ecc_code[i] = chip->oob_poi[eccpos[i]];
    
    	eccsteps = chip->ecc.steps;
    	p = buf;
    
    	for (i = 0 ; eccsteps; eccsteps--, i += eccbytes, p += eccsize) {
    		int stat;
    
    		stat = chip->ecc.correct(mtd, p, &ecc_code[i], &ecc_calc[i]);
    		if (stat < 0)
    			mtd->ecc_stats.failed++;
    		else
    			mtd->ecc_stats.corrected += stat;
    	}
    	return 0;
    }
    
    //ranran ecc
    #if 0
    /**
     * ti81xx_nand_write_page_raw_bch - write raw page according to bch layout
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @buf:	data buffer
     *
     * Not for syndrome calculating ecc controllers, which use a special oob layout
     */
    static void ti81xx_nand_write_page_raw_bch(struct mtd_info *mtd,
    		struct nand_chip *chip, const uint8_t *buf)
    {
    	chip->write_buf(mtd, buf, mtd->writesize);
    	chip->write_buf(mtd, chip->oob_poi, mtd->oobsize);
    }
    
    
    /**
     * ti81xx_nand_read_page_raw - read raw page according to bch layout
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @buf:	buffer to store read data
     * @page:	page number to read
     *
     */
    static int ti81xx_nand_read_page_raw_bch(struct mtd_info *mtd,
    		struct nand_chip *chip, uint8_t *buf, int page)
    {
    	chip->read_buf(mtd, buf, mtd->writesize);
    	chip->read_buf(mtd, chip->oob_poi, mtd->oobsize);
    
    	return 0;
    }
    
    
    /**
     * ti81xx_nand_write_oob_bch - write oob according to bch layout
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @page:	page number to write
     */
    static int ti81xx_nand_write_oob_bch(struct mtd_info *mtd,
    		struct nand_chip *chip, int page)
    {
    	int status = 0;
    
    	chip->cmdfunc(mtd, NAND_CMD_SEQIN, mtd->writesize, page);
    	chip->write_buf(mtd, chip->oob_poi, mtd->oobsize);
    
    	/* Send command to program the OOB data */
    	chip->cmdfunc(mtd, NAND_CMD_PAGEPROG, -1, -1);
    
    	status = chip->waitfunc(mtd, chip);
    
    	return status & NAND_STATUS_FAIL ? -EIO : 0;
    }
    
    /**
     * ti81xx_nand_read_oob_bch - bch hardware ecc based OOB data read function
     * @mtd:	mtd info structure
     * @chip:	nand chip info structure
     * @page:	page number to read
     * @sndcmd:	flag whether to issue read command or not
     */
    static int ti81xx_nand_read_oob_bch(struct mtd_info *mtd,
    		struct nand_chip *chip, int page, int sndcmd)
    {
    	chip->cmdfunc(mtd, NAND_CMD_READ0, mtd->writesize, page);
    	chip->read_buf(mtd, chip->oob_poi, mtd->oobsize);
    
    	return 1;
    }
    #endif
    
    /*
     * ti81xx_enable_ecc_bch- This function enables the bch h/w ecc functionality
     * @mtd:        MTD device structure
     * @mode:       Read/Write mode
     *
     */
    static void ti81xx_enable_ecc_bch(struct mtd_info *mtd, int32_t mode)
    {
    	struct nand_chip *chip = mtd->priv;
    
    	ti81xx_hwecc_init_bch(chip, mode);
    	/* enable ecc */
    	writel((readl(&gpmc_cfg->ecc_config) | 0x1), &gpmc_cfg->ecc_config);
    }
    
    
    /*
     * ti81xx_enable_ecc - This function enables the hardware ecc functionality
     * @mtd:        MTD device structure
     * @mode:       Read/Write mode
     */
    static void ti81xx_enable_ecc(struct mtd_info *mtd, int32_t mode)
    {
    	struct nand_chip *chip = mtd->priv;
    	uint32_t val, dev_width = (chip->options & NAND_BUSWIDTH_16) >> 1;
    
    	switch (mode) {
    	case NAND_ECC_READ:
    	case NAND_ECC_WRITE:
    		/* Clear the ecc result registers, select ecc reg as 1 */
    		writel(ECCCLEAR | ECCRESULTREG1, &gpmc_cfg->ecc_control);
    
    		/*
    		 * Size 0 = 0xFF, Size1 is 0xFF - both are 512 bytes
    		 * tell all regs to generate size0 sized regs
    		 * we just have a single ECC engine for all CS
    		 */
    		writel(ECCSIZE1 | ECCSIZE0 | ECCSIZE0SEL,
    			&gpmc_cfg->ecc_size_config);
    		val = (dev_width << 7) | (cs << 1) | (0x1);
    		writel(val, &gpmc_cfg->ecc_config);
    		break;
    	default:
    		printf("Error: Unrecognized Mode[%d]!\n", mode);
    		break;
    	}
    }
    
    
    
    /*
     * __ti81xx_nand_switch_ecc - switch the ECC operation ib/w h/w ecc
     * (i.e. hamming / bch) and s/w ecc.
     * The default is to come up on s/w ecc
     *
     * @nand:	NAND chip datastructure
     * @hardware:  NAND_ECC_HW -switch to h/w ecc
     * 				NAND_ECC_SOFT -switch to s/w ecc
     *
     * @mode: 		0 - hamming code
     * 				1 - bch4
     *				2 - bch8
     *				3 - bch16
     *
     * @return: 0 - success, or error
     */
    int __ti81xx_nand_switch_ecc(struct nand_chip *nand,
    		nand_ecc_modes_t hardware, int32_t mode)
    {
    	struct nand_bch_priv *bch;
    	int ret = 0;
    
    	bch = nand->priv;
    	nand->options |= NAND_OWN_BUFFERS;
    
    	/* Reset ecc interface */
    	nand->ecc.read_page = NULL;
    	nand->ecc.write_page = NULL;
    	nand->ecc.read_oob = NULL;
    	nand->ecc.write_oob = NULL;
    	nand->ecc.hwctl = NULL;
    	nand->ecc.correct = NULL;
    	nand->ecc.calculate = NULL;
    
    	nand->ecc.write_page = NULL;
    	nand->ecc.read_page = NULL;
    	nand->ecc.mode = hardware;
    	/* Setup the ecc configurations again */
    	if (hardware == NAND_ECC_HW) {
    		if (mode) {
    			bch->mode = NAND_ECC_HW_BCH;
    			/* -1 for converting mode to bch type */
    			bch->type = mode - 1;
    			printf("HW ECC BCH");
    			switch (bch->type) {
    				case ECC_BCH4:
    					nand->ecc.layout = &hw_bch4_nand_oob;
    					bch->nibbles = ECC_BCH4_NIBBLES;
    					nand->ecc.bytes = 8;
    					printf("4 not supported\n");
    					ret = -EINVAL;
    					goto no_support;
    					break;
    				case ECC_BCH16:
    					nand->ecc.bytes = 26;
    					nand->ecc.layout = &hw_bch16_nand_oob;
    					bch->nibbles = ECC_BCH16_NIBBLES;
    					printf("16 not supported\n");
    					ret = -EINVAL;
    					goto no_support;
    					break;
    				case ECC_BCH8:
    				default:
    					nand->ecc.bytes = 14;
    					nand->ecc.layout = &hw_bch8_nand_oob;
    //ranran ecc
    #if 0
    					nand->ecc.read_page_raw =
    						ti81xx_nand_read_page_raw_bch;
    					nand->ecc.write_page_raw =
    						ti81xx_nand_write_page_raw_bch;
    					nand->ecc.read_oob =
    						ti81xx_nand_read_oob_bch;
    					nand->ecc.write_oob =
    						ti81xx_nand_write_oob_bch;
    #endif
    					bch->nibbles = ECC_BCH8_NIBBLES;
    					printf("8 Selected\n");
    					break;
    			}
    			bch->mode = NAND_ECC_HW;
    			nand->ecc.mode = NAND_ECC_HW_SYNDROME;
    			#ifdef CONFIG_UD8168_DVR
    			if(dvr_get_hw_version() < 0x3a)
    				nand->ecc.steps = 8;
    			else
    			nand->ecc.steps = 4;
    			#endif
    
    			nand->ecc.size = 512;
    			nand->ecc.total = (nand->ecc.steps * nand->ecc.bytes);
    			nand->ecc.write_page = ti81xx_write_page_bch;
    			nand->ecc.read_page = ti81xx_read_page_bch;
    			nand->ecc.hwctl = ti81xx_enable_ecc_bch;
    			nand->ecc.correct = ti81xx_correct_data_bch;
    			nand->ecc.calculate = ti81xx_calculate_ecc_bch;
    			ti81xx_hwecc_init_bch(nand, NAND_ECC_READ);
    		} else {
    			bch->mode = NAND_ECC_HW;
    			#ifdef CONFIG_UD8168_DVR
    			if(dvr_get_hw_version() < 0x3a)
    				nand->ecc.layout = &hw_nand_oob_p4k;
    			else
    				nand->ecc.layout = &hw_nand_oob;
    			#else
    			nand->ecc.layout = &hw_nand_oob;
    			#endif
    			nand->ecc.size = 512;
    			nand->ecc.bytes = 3;
    			nand->ecc.hwctl = ti81xx_enable_ecc;
    			nand->ecc.correct = ti81xx_correct_data;
    			nand->ecc.calculate = ti81xx_calculate_ecc;
    			ti81xx_hwecc_init(nand);
    			printf("HW ECC Hamming Code selected\n");
    		}
    	} else if(hardware == NAND_ECC_SOFT) {
    		/* Use mtd default settings */
    		nand->ecc.layout = NULL;
    		printf("SW ECC selected\n");
    	} else {
    		printf("ECC Disabled\n");
    		ret = -EINVAL;
    	}
    
    no_support:
    	return ret;
    }
    
    
    /*
     * ti81xx_nand_switch_ecc - switch the ECC operation ib/w h/w ecc
     * (i.e. hamming / bch) and s/w ecc.
     * The default is to come up on s/w ecc
     *
     * @hardware -  NAND_ECC_HW -switch to h/w ecc
     * 				NAND_ECC_SOFT -switch to s/w ecc
     *
     * @mode - 		0 - hamming code
     * 				1 - bch4
     *				2 - bch8
     *				3 - bch16
     *
     *
     */
    void ti81xx_nand_switch_ecc(nand_ecc_modes_t hardware, int32_t mode)
    {
    	struct nand_chip *nand;
    	struct mtd_info *mtd;
    
    	if (nand_curr_device < 0 ||
    	    nand_curr_device >= CONFIG_SYS_MAX_NAND_DEVICE) {
    		printf("Error: Can't switch ecc, no devices available\n");
    		return;
    	}
    
    	mtd = &nand_info[nand_curr_device];
    	nand = mtd->priv;
    
    	if (0 == __ti81xx_nand_switch_ecc(nand, hardware, mode)) {
    		/* Update NAND handling after successful ECC mode switch */
    		nand_scan_tail(mtd);
    	}
    	nand->options &= ~NAND_OWN_BUFFERS;
    
    	return;
    }
    
    /*
     * Board-specific NAND initialization. The following members of the
     * argument are board-specific:
     * - IO_ADDR_R: address to read the 8 I/O lines of the flash device
     * - IO_ADDR_W: address to write the 8 I/O lines of the flash device
     * - cmd_ctrl: hardwarespecific function for accesing control-lines
     * - waitfunc: hardwarespecific function for accesing device ready/busy line
     * - ecc.hwctl: function to enable (reset) hardware ecc generator
     * - ecc.mode: mode of ecc, see defines
     * - chip_delay: chip dependent delay for transfering data from array to
     *   read regs (tR)
     * - options: various chip options. They can partly be set to inform
     *   nand_scan about special functionality. See the defines for further
     *   explanation
     */
    int board_nand_init(struct nand_chip *nand)
    {
    	/* int32_t gpmc_config = 0; */
    	cs = 0;
    
    	/*
    	 * xloader/Uboot's gpmc configuration would have configured GPMC for
    	 * nand type of memory. The following logic scans and latches on to the
    	 * first CS with NAND type memory.
    	 * TBD: need to make this logic generic to handle multiple CS NAND
    	 * devices.
    	 */
    	while (cs < GPMC_MAX_CS) {
    		/* Check if NAND type is set */
    		if ((readl(&gpmc_cfg->cs[cs].config1) & 0xC00) == 0x800) {
    			/* Found it!! */
    #ifdef NAND_DEBUG
    			printf("Searching for NAND device @ GPMC CS:%1d\n", cs);
    #endif
    			break;
    		}
    		cs++;
    	}
    	if (cs >= GPMC_MAX_CS) {
    		printf("NAND: Unable to find NAND settings in "
    			"GPMC Configuration - quitting\n");
    		return -ENODEV;
    	}
    
    	nand->IO_ADDR_R = (void __iomem *)&gpmc_cfg->cs[cs].nand_dat;
    	nand->IO_ADDR_W = (void __iomem *)&gpmc_cfg->cs[cs].nand_cmd;
    
    	nand->cmd_ctrl = ti81xx_nand_hwcontrol;
    	nand->options = NAND_NO_PADDING | NAND_CACHEPRG | NAND_NO_AUTOINCR;
    	/* If we are 16 bit dev, our gpmc config tells us that */
    	if ((readl(&gpmc_cfg->cs[cs].config1) & 0x3000) == 0x1000) {
    		nand->options |= NAND_BUSWIDTH_16;
    	}
    
    	nand->chip_delay = 100;
    
    	/* fallback ecc info, this will be overridden by
    	 * ti81xx_nand_switch_ecc() below to 1-bit h/w ecc
    	 */
    	nand->priv = &bch_priv;
    	nand->ecc.mode = NAND_ECC_SOFT;
    
    	/* required in case of BCH */
    	elm_init();
    
    	nand_curr_device = 0;
            //ranran ecc
    #if 0
            ti81xx_nand_switch_ecc(NAND_ECC_HW, 2);
    #else
            ti81xx_nand_switch_ecc(NAND_ECC_HW, 0);
    #endif
    	return 0;
    }
    
    

    I wander what I'm doing wrong.

    Best Regards,

    Ran

  • Hello,

    For anyone from e2e community who is also interested:
    I've managed to work with hamming hw ecc and jffs.
    The patches I've used and the scheme I've used were all correct, except for the scheme for programming u-boot 1st stage:
    It should be programmed as BCH8 (as I wrote in my previous message), The reason for that , as I understand is that the ROM use ecc BCH8.

    Thank you,
    Ran
  • Ran Shalit said:
    The patches I've used and the scheme I've used were all correct, except for the scheme for programming u-boot 1st stage:
    It should be programmed as BCH8 (as I wrote in my previous message), The reason for that , as I understand is that the ROM use ecc BCH8.

    This might be DVR RDK specific. I can successfully program the u-boot 1st stage with Hamming (ROM Code is BCH8), and EVM boots fine.

    Regards,
    Pavel