On some boards with a DM8168, we have a strange reboot problem.
We issue the "reboot" command on linux console... The system is shutting down and we see the RSTOUTn signal going low (byt hte way wehre are the timings of this signal, i could not find it on data sheet or ref manual), then the signal is going up .. this means that the RST internal from PCM is released...
but that's it..nothing more. the bootloader doen's start and the system is freezed. But if i pres the reset button (activating the REsetn or POR signal) the system start correctly.
Waht could be wrong ? not al the boards has this problem.... just some of them.
The two signal PRO and REsetn are pullupped and stay stable during console "reboot"..
Thanks
Omar