This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x evm boot from SD

Hello,

I'm new to am335x evm board and I need help to solve a problem with booting from SD.

Steps I do:

1. Insert Linux SD card (from the box) in slot0

2. Set up SD boot mode as decribed in processors.wiki.ti.com/.../AM335x_U-Boot_User%27s_Guide

3. Power on the board.

And the only thing that I can see in TeraTerm is 'CCCCC' symbols. I've tried with Android card and there is the same result.

I've also tried to boot from NAND and there were messages:

- mmc_send_cmd : timeout: No status update

- Card did not respond to voltage select!

Thank you in advance,

Alexey.