Other Parts Discussed in Thread: OMAP3530
Dear All:
UART1 of DM365 is using GPIO15 and GPIO16 pins, but the same pins are used by EMAC.
We found that there are GPIO34 and GPIO25 which seem to be able to configure as UART1RX and UART1TX, too.
I have modified the pinmux configuration of the Linux kernel to use these two pins, but it failed.
Is it possible to use GPIO34 and GPIO25 as UART1?
We really like to use EMAC and UART1 at the same time.
If it is possible, how shall I proceed?
Is there anything need to be modified in addition to the pinmux configuration?
Thank you in advance.
Best regards,
Ray