Hello,
I'm trying to boot the C6748 on a custom board using TI UartHost Utility. My application contains NDK package, through which I have UDP communication. I have the application running perfectly on the debugger using the GEL file. I'm using the AISgen tool to get the .bin file. When I use the UartHost utility, the boot is successful, but the board becomes unresponsive. After many attempts, I figured out that, when I add the NDK to the project and boot it, the board becomes unresponsive(but boot is successful). But the same project runs fine on the debugger. So it should be some configuration which I'm doing in the AISgen, which is causing problems. I tried to match everything from my GEL file to the AISgen configuration, but it didn't help. Strangely, my application without the NDK boots perfectly. So my guess here is some memory mapping issue, when NDK is used in the project. I have attached my AISgen configuration file and my GEL file below. Can anybody help me with this problem?
Device type: d800k008
mDDR memory