Hello,
I would please like your advise, about using streamer with DM8148.
I need to use DM8148 for demux of MPEG-TS and decoding of H.264 for display (simple single chain of etherenet(MPEG-TS)->decode(H.264)->display.
I would like to ask how would you recommend to build it in software, which of the following is preferred ?
1. using ezsdk framework (with gstreamer)
2. using dvrrdk framework (which demux can be used here) ?
There is also strict requirement for the latency (~150msec end to end)
Thank you for the any suggestions,
Ran