This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[Primus] CVDD looks leaked to DVDD during power up sequence



Hi,

My customer is now launching their HW using DA810.
 
Please assume the power up sequence is exactly following the description of Power-On Sequence in the data sheet.
That looks like :
- All of 1.2V (CVDD and related power supplies as RTC_CVDD and PLL0_VDDA) lane is powered on
- After CVDD is reached to the operating condition, DVDD is powered on. (Please note 1.8V power supply is not being used for USB0_VDDA18 because they does not use USB0) 
- During the above power up sequence, /RESET pin is always being asserted (LOW). /RESET pin will be de-asserted once DVDD is reached to the operation condition.

So the question is, when CVDD is powered on, they saw some leak voltage (0.47V) on DVDD. Is this correct behavior ?

Best Regards,
Kawada