Other Parts Discussed in Thread: SYSBIOS
Hardware : Tiva C series DK-TM4C129x board with TI-RTOS
I was going through the GPIO interrupt example for the above board and came across the function hwi_construct used to setup the callback for interrupt handling.
Also, I was going through Hardware interrupts section in the SYS-BIOS 6.41 user guide. there is no mention of hwi_construct. but they mention the the following
APIs
hwi_register, hwi_create, etc,,,
I would like to write minimal code in ISR and do the post-processing using SWI by using swi_post (eg. for a packet I receive on UART).
Any tutorial or example code to help me understand of using HWI and SWI together.
TIA
Narendra