This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eSATA driver issue while using NTFS on dm6467

Hi all,

I have a eSATA drive connected to dm6467,it's NTFS filesystem.  now I can read data from this drive, but can not write data into it.

then I port ntfs-3g (ntfs-3g-2010.3.6) to arm,but i have some problems
    1. First i compiler the fuse-2.8.3.tar.gz to get a fuse.ko and insmod fuse.ko
       to linux kernel(not select : ntfs file system support in menuconfig)
    2. Connected the esata harddisk to eSATA port ,not messgs display ,for example
       esata -  /dev/hdb1 ...
    so, i restart the linux kernel,and i am used the command: fdisk -l ,just nothing
    to been display
   
    The most important:
    Selected the ntfs file system support in menuconfig,
    so, restart the linux kernel,and i am used the command: fdisk -l
    //-------------------------------
    root@dm6467-evm:~#
  root@dm6467-evm:~# fdisk -l | grep NTFS
  /dev/hdb1   *           1        6225    50002281    7  HPFS/NTFS
  /dev/hdb5            6226       12753    52436128+   7  HPFS/NTFS
  /dev/hdb6           12754       30394   141701301    7  HPFS/NTFS
  //-------------------------------
  but just
  root@dm6467-evm:/media# ls -l
  dr-x------    1 root     root         8192 Feb 25  2010 hdb1
  dr-x------    1 root     root        28672 Apr  9  2010 hdb5
  dr-x------    1 root     root         4096 Apr  9  2010 hdb6
  not support write
  //-------------------
  i get some messages that linux kernel just support read the NTFS not write,
   if write error may  linux kernel crash, i try it.it happens on dm64467 (linux kernel 2.6.32)
   
   is there anyone can help me?
  
I use DVSDK3.10

 

Thanks,

Rain