Hi,
I am launching program on DSPs from ARM cores. In case there is bug in the code, most of the time the Ctrl-C will not be able to kill the running code and I have to manually reboot the DSP. I tried login to BMC (via ttyUSB1) but don't see commands like "bootmode", "reboot" available there. It says command not found. Can you please suggest how to reboot remotely using BMC terminal? Copying the BMC "ver" command o/p:
BMC>ver
BMC Version EVM Type EVM Superset EVM Subset EVM Version EVM S/N
1.0.1.3a 0.0.0.1 K2KH-EVM XTCIEVMK2X 1.0.0.1 15048
Also, for the cases where I am able to kill frozen program using Ctrl-C, I see that any further launch of correct (pre-working) code also hangs but works fine after a reboot of evm.
Thanks & Regards
Vivek Kumar