This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM437x wake up time

Guru 16800 points
Other Parts Discussed in Thread: TIDEP0024

Hello,

In the following page, Wakeup time for Suspend GPIO (ms) is 308.61 (min 303.32, max 310.06) is described.
http://processors.wiki.ti.com/index.php/Sitara_Linux_SDK_Kernel_Performance_Guide#Wakeup_Times_2

I have two questions for the time.

1. When DRAM is changed from DDR3 to LPDDR2 (266MHz), please let me know how wake up time is long.
   I think the wakeup time is longer than the case of using DDR3.

2. Please let me know the definition of "Wakeup time".
   Does the time include the peripheral setting time?

Best Regards,

Nomoto