Hi,
We have been using a custom Platform file create by RTSC Platform tool for our C66x based product.
Recently, I modified the file a bit using the tool and suddenly the system started behaving strangely. It turned out that the generated platform file now uses different XDC tool version (originally it was 3_25_00_48 and now it is changed to 3_30_01_25. In my environment, both are installed).
The DSP .out project uses 3.25.0.48.
So, my question is, how do you force the XDC version in Platform file?
I use CCS v5.4.0.00091, and I have both 3_25_00_48 and 3_30_01_25 XDC installed.
Thanks,
tamo2