Other Parts Discussed in Thread: OMAPL138
Hello, I am using the TMS320C6748LCDK for my application. I need to store an image and hence need more memory. I am using a sample code to read the data from the cameras buffer. When I try to run the code with the amount of required memory it says unable to access memory location. Is the default memory allocation less than the complete allocation? How can I change the allocation?