This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS6.1 fails when compiling OMAP4460 C64x example project



Running Windows 7 64-bit, CCS 6.1.0.00104

Created new project:

Target: OMAP4460

Tab: C64XX

Compiler version: TI v7.4.14

Output type: Executable

Output format: eabi (ELF)

Device endianness: little

Linker command file: <none>

Runtime support library: <automatic>

Project templates and examples: TI-RTOS for C6000/Kernel Examples/Minimal

XDCtools version: 3.31.0.24_core

Products and Repositories: TI-RTOS for C6000 2.0.1.23

Target: ti.targets.elf.C64T

Platform: sdp4430 (the closest I could find)

Build-profile: release

I immediately try to build the project, and get the error  "can't find the library 'lib/ti.targets.rts6000.ae64T' specified by package ti.targets.rts6000"

Can someone please tell me what I'm doing wrong?

Thanks,

Jonathan