hello all, I am working on DM648 with ndk1.92. I want to implement an intelligent switch application with the involvement of DSP processor of the topology mentioned below
data from LAN ----->port0 (PHY 1) of dsp ------>port2( DSP processor) --------->port1(PHY 2) --------> to the PC
and similarly
To LAN <-----port0 (PHY 1) of dsp <------port2( DSP processor) <---------port1(PHY 2) <-------- data from PC
in a full duplex fashion. Now could u plz guide which NDk program i.e (cfgdemo,client , hello world or anyother ) should I use.
I had tried alot on helloworld application but it has been configured in normal mode(i.e data do not go to DSP ) do anybody know how to configure it in bypass mode?
Note that I do not need DHCP,HTTP or any other server client application out of it.
Waiting for ur reply
Regards
Ahmed