Other Parts Discussed in Thread: 66AK2E05, TPS544C20, TPS544C25
Dear whom may it concern,
I am making a custom board with 66AK2E05 processor from K2E EVM. K2E EVM uses TPS544C24 power converter, but it is not available.
The other thread on this forum says that uses TPS544C20 instead of TPS544C24 while TPS544C20 is not functionally compatible with TPS544C24. It also said that TPS544C25 is a functional compatible with TPS544C24, but it is a sample stage. I cannot find any information of TPS544C25. Can I get the sample of TPS544C25 or buy it?
I compared TPS544C20 to TPS544C24 on K2E schematic, and I found that pin 13, 30, and 39 has different pin name and function.
Is it possible to use a TPS544C20 instead of TPS544C24 without a modification on the circuit in K2E schematic? or should I modified the circuit based on the schematic of the TPS544C20 EVM?
Regards,
Jaehyun Park