This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x capture/encode of multiple different sources

Guru 20755 points


Hello,

I have requirement to encode the following input together. I would like to ask if it is feasable with DM814x:

1. how should I input the sources into VIP ?
2. Does HDVPSS and HDVICP can handle all the 6 sources together ?


ID Video Source Name                           Full Rate                      MByte / Sec Single JP2 Bytes JP2 @30Hz MByte/Sec
1. Sensor 1 (CCD) Raw Images            720x704x2 60Hz 60 128K       4
2. Sensor 1 (CCD) Processed Images 640x480x1 30Hz 10 48K         1.5
3. Sensor 2 (FLIR) Raw Images            640x512x2 60Hz 40 128K       4
4. Sensor 2 (FLIR) Processed Images 640x480x1 30Hz 10 48K         1.5
5. Sensor 3 (SNS) Processed Images 640x480x1 30Hz 10 48K         1.5
5. Monitor Images (with symbols)         640x480x1 30Hz 10 48K         1.5

Best Regards,

Ran