Hello,
Please let me know the definition of BALL RESET STATE and BALL RESET REL. STATE described on page 17 of datasheet.
In datasheet, "H" means High-impedance with an active pull-up resistor.
Therefore, the GPIO pin which has the "H" state should be High during executing ROM code, because the ROM code doesn't change IO state.
However, some GPIO pins such as gpio1_28 (U18 on ZCZ) is 1V or 2V during executing ROM code.
GPIO connects to the FET gate pins; therefore the voltage shouldn't be dropped.
Could you tell me why the voltage drops?
Best Regards,
Nomoto