This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTSC module access problem



Dear,

I'm building an application with CCS4.

I have a project with a linked RTSC project.

Up to know, everything compiles and links correctly, however I want to use DSP/BIOS and I want to start using the "Mailbox" module

I have two questions:

QUESTION 1:

 I click on my project.cfg file in the RTSC project and add the Mailbox module to my configuration. I subsequently add a Mailbox instance to the module. Everything still compiles and links correctly

How can I from within my C++ code, access the created mailbox, since I don't have the handle to it.

 

QUESTION 2:

Since I did not know how to get a handle to the object, I considered that maybe as per "spru403g" which is the "TMS320C6000 DSP/BIOS Application Programming Interface
(API) Reference Guide" I can do the work myself. So I add the code to my application. I have access to all include files and all definitions seem to be correct.

The application compiles without a problem, but when linking I get the message:

Undefined symbol "_MBX_Create"

the other functions are found correctly (because in the include file, they are just macros to the built in code)

What do I have to do to get the app to link correctly the _MBX_Create into the app

thanks for your support

Marc