This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517 MDIO reinitialization

Genius 5785 points


Hello,

I'd like to re-initialize MDIO module in order to search the PHY connected to MDIO. I'll clear to 0 in ENABLE-bit of MDIO Control Register. Then I'll set to 1 in it and configure PREAMBLE and CLKDIV concurrently. I think this operation leads to start searching for the PHY by MDIO module. Do I also need to re-initialize EMAC subsystem module by setting SOFTRESET Register?

Regards,
Kazu