Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi!
The following sentences are from the link processors.wiki.ti.com/.../Rebuilding_the_Flash_and_Boot_Utils_Package
ARM Compiler Tools (CodeSourcery G++ Lite)
- Download the ARM compiler tools here: http://www.codesourcery.com/sgpp/lite/arm/portal/subscription3057
- If using v2.40 or later: Edit the Common/build.mak file to have the correct ARM_TOOLS_PATH and ARM_TOOLS_PREFIX variables
- If using v2.36 or earlier: Add the bin directory of the ARM cross-compiler tools to the system path environment variable.
so I click the link and just don't know what exactly I should download, I filled some names, addresses etc.And in the end, just got a page telling me to check the email and I got nothing.So what should I do?Thanks!