Hi all,
We have a custom board based on DM8168 with a Micron MT41K128M16JT DDR3 running at 796MHz. We have a gstreamer application that makes dual capture (1080p@30) and dual display, also it is scaling and encoding each one. We are facing random failures, sometimes the board runs fine and sometimes we got a kernel crash but this kernel crash is not consistent, we don't get the same kernel error in each crash. We think that it is something related with memory corruption, similar to the problem found in the following post:
We don't think it is a software related issue because we ran the same test in a DM8168 EVM board and it didn't crash, so we discarded a software issue. How can we determine if it is a memory corruption issue? Is there a way to do it using CCS?
We are using the EZSDK 5.05.02.
Thanks,
Eugenia