Hi,
I've no problem booting on uart2, but when I try through uart1 then sfh_OMAP-L138 tool hangs after printing: "Waiting for SFT on the OMAP-L138..."
chip: C6748
Screenshot:
-----------------------------------------------------
TI Serial Flasher Host Program for OMAP-L138
(C) 2010, Texas Instruments, Inc.
Ver. 1.67
-----------------------------------------------------
[TYPE] Global erase
[TARGET] C6748
[DEVICE] SPI_MEM
Attempting to connect to device COM3...
Press any key to end this program at any time.
(AIS Parse): Read magic word 0x41504954.
(AIS Parse): Waiting for BOOTME... (power on or reset target now)
(Serial Port): Read error! (The operation has timed out.)
(AIS Parse): BOOTME received!
(AIS Parse): Performing Start-Word Sync...
(AIS Parse): Performing Ping Opcode Sync...
(AIS Parse): Processing command 0: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 15296-Byte section to address 0x11800000.
(AIS Parse): Processing command 1: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 736-Byte section to address 0x11803BC0.
(AIS Parse): Processing command 2: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 32-Byte section to address 0x11803EA0.
(AIS Parse): Processing command 3: 0x58535901.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Loading section...
(AIS Parse): Loaded 20-Byte section to address 0x11803EE0.
(AIS Parse): Processing command 4: 0x58535906.
(AIS Parse): Performing Opcode Sync...
(AIS Parse): Performing jump and close...
(AIS Parse): AIS complete. Jump to address 0x118036A0.
(AIS Parse): Waiting for DONE...
(AIS Parse): Boot completed successfully.
Waiting for SFT on the OMAP-L138...
Keeps on waiting for something here...
Best regards,
Bruno