Hello,
I have some general question regarding cpu usage and ethernet:
I have reviewed the performance and feature wiki for DM814X:

It shows that when ethernet TX reaches ~300Mbit/sec the cpu load is about 100%
and if ethernet RX reaches ~410Mbits/sec , then cpu load is about 90%.
Does anyone knows why is can't reach the 1Gbits/sec, and why cpu usage reaches maximum when ethernet useage is far below the 1Gbits/sec capacity ?
Thank you,
Ran