This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 - RAM copy issue

Hello,

We are facing an issue for copying the binary file larger than RAM size. We are using u-boot-2011.09 version. At u-boot, we are copying the binary image(UBI File System Image) from SD Card to the RAM first and then to the NAND Flash. The RAM is of 64MB and the NAND Flash is of 128 MB. We are unable to copy the binary that is more than 58 MB (As RAM is 64MB). We have a requirement to copy the binary that is of higher size (> 70 MB). Can someone please help regarding an alternate solution to do so. Is there any flash utility to copy the binary directly on NAND Flash?


Thanks,

Hareesh M