This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB Host problem in dm365.



Hi,

We are using dm365 with kernel 2.6.37 of  IPNC_RDK_DM36x_V5.1.0.

We had configured USB as only host from kernel.

While testing we found out that, when we connect any mass storage device to usb port at boot time then its is being detected correctly and works fine.

Even in same session (without rebooting board) if we remove and insert then it is being detected and works perfectly.

But if connect same mass storage after it boots completely then its not being detected. It is not being detected in if we do not connect it while booting time. 

Can you help us. What we are missing to configure so that it works with plug and play also.

Thanks.