Good day experts,
I am referring to my previous thread (which appears to have been closed):
I would like to port the McBSP driver from the most recent C6748 PDK (v2.00, 24 May 2012) to the C6657 so that I can use the PING-PONG configuration. From what I could gather, the McBSP peripheral is identical on both platforms so I suspect the only significant difference would be the peripheral configuration through the CSL and perhaps the way interrupts are handled?
Are there any other pitfalls that I should be aware of?