Hi all:
I use dm8618 dvrrdk4.0.
In my application i capture 1080P 60 Hz video and output use display link,
Only capture link and display link used, and the time delay is about 60 ms,
ISRFlag i have set true already.
and i see the log, the min/max display link is 50/75,
i want to know why display cost so much time,
is there lots of functions in hdvpss which i do not need opened?
And how can i lower the display time delay for my application.