This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I cant't find two head file,please help!



Hi all:

    I download KeyStone 2 Self Test Kit,I follow the user guide to add PDK path to Include Options,The user guide says that  

   You may need to change the CSL including path, by default the project use CSL header files in: C:\ti\pdk_keystone2_3_01_01_04\packages\ti\csl

   but in my install path, the real path is C:\ti\pdk_C6678_1_1_2_5\packages\ti\csl 

   I add it to the project and the compiler post fatal error

  "D:/Test_EVM/K2_STK_DSP_v1.1/common/K2_common.h", line 57: fatal error #5: could not open source file "cslr_tetris_vbusp.h"

  I search this file in the path C:\ti, but there is no result.

  These files can not be found 

    <csl_device_interrupt.h>
    <cslr_tetris_vbusp.h>

  where can I get these two file?

   Thank you 

  Best Regards

Yewkui Wang