Other Parts Discussed in Thread: OMAP-L138
I found a possible bug in the OMAP-L138 Starterware timer routines. Perhaps it's not a full-on bug, but it's unclean, and may need fixing.
In the file \drivers\timer.c, in the routine, TimerConfigure(), there is the following line of code:
HWREG(baseAddr + TMR_TCR) = (config & (TMR_TCR_CLKSRC12 | TMR_TCR_CLKSRC34));
The item in red (along with config) can potentially set bit-24 of the Timer Control Register (TCR). However, in the OMAP-L138, that bit is RESERVED, and should be zero, not set to one. (Reference: OMAP-L138 Tech Ref Manual)
I don't know if that actually causes a problem. (Setting a reserved bit to one.) At the least, it's unclean.
The clean solution is to:
- Delete | TMR_TCR_CLKSRC34 from that line of code for this processor. Or,
- Use an #if <processor-type> in that file to insert the correct line of code, depending on processor-type. Or,
- Use an #if <processor-type>, (in the header file, hw_tmr.h) to #define it to zero for this processor.
Can a TI person verify this for us?
-- Walter Snafu