This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm trying to implement DDR3 initialization as per SPRABX7 ("Keystone II DDR3 Initialization").
On "Example 4. DDR PHY Initialization"
//Assert DDR PHY reset after PLL enabled DDR3APLLCTL1 = DDR3APLLCTL1 | 0x80000000; for(i=0;i<delay;i++); DDR3APLLCTL1 = DDR3APLLCTL1 & 0x7FFFFFFF; //Release DDR PHY reset
SPRS866E states (page 307) that DDR3APLLCTL1 bit 31 is reserved, not phy reset as the code snippet suggests.
On DDR3 manual (SPRUHN7C) I can find two different PHY reset bits:
PIR bit 6 (PHYRST); and
PGCR1 bit 25 (PHYHRST).
1. What is the proper PHY reset sequence needed before polling IDONE?
BR, -Topi