This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDK 8.0 pre-built images broken?

After installing SDK 8.0 and running create-sdcard.sh with pre-built option, resulting sdcard boots Debian. I'm suspecting the sdcard did _not_ boot and instead the default BeagleBone Debian image booted from emmc. The sdcard boot and rootfs partitions appear to be intact. Console shows:

U-Boot SPL 2014.04-00014-g47880f5 (Apr 22 2014 - 13:23:54)
reading args
spl_load_image_fat_os: error reading image args, err - -1

If the SDK pre-builds are indeed broken, is there a workaround or repository where updated prebuilds can be acquired.?

Thanks